Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Xilinx Tools vrs ZedBoard Vrs Windows8
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 252 views
  • Users 0 members are here
Related

Xilinx Tools vrs ZedBoard Vrs Windows8

Former Member
Former Member over 12 years ago

I just received my Zedboard, I want to follow the ZEDBOARD training videos, the labs etc. I cannot find the "PlanAhead" software.

I did not use the DVD (my laptop does not have a DVD/CD) so I downloaded the latest version from Xilinx un-tared it and ran the setup.exe.

I have tried the WebPack, the System Version, and multiple others with little to no luck.

I get several icons on the desktop, the problem one is Vivado 2013.4 - I click this, and nothing happens. I get a dead process running in the background I can kill with task manager.

If I run the batch file as below, I get an error message that GUI is not supported on windows?

I am stuck, any suggestions?

Is there another way to get the PlanAhead SW?


c:xilinxVivado2013.4bin>vivado.bat

****** Vivado v2013.4 (64-bit)
  **** SW Build 353583 on Mon Dec  9 17:49:19 MST 2013
  **** IP Build 208076 on Mon Dec  2 12:38:17 MST 2013
    ** Copyright 1986-1999, 2001-2013 Xilinx, Inc. All Rights Reserved.

Attempting to get a license: Implementation
Feature available: Implementation
Loading parts and site information from c:/xilinx/Vivado/2013.4/data/parts/arch.xml
Parsing RTL primitives file [c:/xilinx/Vivado/2013.4/data/parts/xilinx/rtl/prims/rtl_prims.xml]
Finished parsing RTL primitives file [c:/xilinx/Vivado/2013.4/data/parts/xilinx/rtl/prims/rtl_prims.
xml]
start_gui
ERROR: [Common 17-612] start_gui is not supported on Windows8.
Vivado%

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    The short answer is that Xilinx tools are not officially supported under Windows 8, just Windows 7, Windows XP and Linux:

    http://www.xilinx.com/ise/ossupport/index.htm

     

    Now the long answer. There are workarounds posted on the Xilinx forums and other sites for both the Vivado and ISE/PlanAhead tool chains that are reported to have mixed results such as:

    http://forums.xilinx.com/t5/Installation-and-Licensing/Xilinx-ISE-installation-problem-on-windows8-Release-Preview/td-p/245650/page/4

     

    Your best bet is to run the tools under Win 7 or Linux if possible, even if you need to do this in a virtual machine within your Windows 8 OS.

     

    Now to 'PlanAhead'. There are currently two Xilinx tool suites, the newer Vivado suite that supports the '7 Series' devices (Including the Zynq device on the ZedBoard) and the older ISE design tools. PlanAhead is part of the ISE tool suite so downloading ISE will get you PlanAhead. Much of the current material on ZedBoard.org was done in the ISE/PlanAhead but all new material will be done using the Vivado tools as will new material from Xilinx. My understanding is that the ISE design tools last update was version 14.7 and that there may not be any further updates. I would encourage you to start any new development using the Vivado tools.

     

    As a note, you can install both the ISE and Vivado tools on the same machine and use either one. You license should work with both tools.

     

    -Gary