Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Vivado HDMI reference design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 370 subscribers
  • Views 1078 views
  • Users 0 members are here
Related

Vivado HDMI reference design

e14 Contributor
e14 Contributor over 12 years ago

Xilinx Vivado Design Suite 2013.2 is out, with Zynq support for IP Integrator.
I was successful with the basic tutorial (http://www.xilinx.com/support/documentation/sw_manuals/xilinx2013_1/ug940-vivado-tutorial-embedded-design.pdf), I've created a sample LED blinking project.
Unfortunately, I am stuck with the HDMI output controller. I've imported the EDK HDMI cores (axi_clkgen, axi_hdmi_tx_16b), but I am unsure what to do next, which interface should I connect to where, etc.
For example: the XPS Linux reference design (http://digilentinc.com/Data/Products/ZEDBOARD/ZedBoard_Linux_Design.zip) connects the M_AXIS_MM2S interface of the VDMA with the M_AXIS_MM2S interface of the HDMI_TX. Vivado does not allow this connection. Also, the Vivado VDMA core does not have the mm2s_fsync_out wire, so I can't connect it to vdma_fs_ret in the HDMI core.

My question is: is there a ZedBoard reference design for Vivado, or a step-by-step guide to create a HDMI output design (in XPS) so that I can be sure that I am doing the right thing?

Regards,
Gabor

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I'd like to second this request. Its frustrating that everyone suggests moving to Vivado rather than XPS/PlanAhead with new designs, but there are none of the custom sources and not half as many tutorials.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Gabor,
    I'm also working on a port of AD's reference design cf_adv7511_zed to Vivado. I also couldn't find it online and decided to create it myself based on the existing design for ISE-XPS.
    While doing that I ran into the same two problems you mentioned and this is how you can get around it:

    1. M_AXIS_MM2S interface: when you package up axi_hdmi_tx_v1_0 it automatically chooses port m_axis_mm2s to be a master port based on the M_ prefix. However, when you look at the individual port directions (e.g. m_axis_mm2s_tdata is input just like in a slave interface) this interface is clearly an axi_stream_slave interface and not a master. I don't understand why they called it M_AXIS_MM2S and not S_AXIS_MM2S. In IPI you can manually change the m_axis_mm2s inferface to slave in the 'IP Interfaces' section. After that is done you can connect it to the VDMA core just like in the reference design.

    2. The mm2s_fsync signal is a hidden port in the VDMA core and you can re-enable it with the TCL command:
    set_property -name {CONFIG.C_ENABLE_DEBUG_INFO_1} -value {0} -objects [get_bd_cells axi_vdma_0]
    For further reading you can refer to Xilinx VDMA design guide at http://www.xilinx.com/support/documentation/ip_documentation/axi_vdma/v6_0/pg020_axi_vdma.pdf

    Regards,
    - Arnd

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Gabor,
    Have you succeeded with HDMI controller in Vivado.
    If yes can you kindly guide me?
    I implemented the basic led blinking for zedboard and understood about the u-boot.

    Now i want to implement a basic HDMI project and draw some basic shapes like (circle, triangle etc).

    Regards
    Hamid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you so much for this post. It got me unstuck!

    By the way, if anyone reading this is using the AD-FMCOMMS1 design with Zedboard under Vivado, it looks like Analog Devices is about to re-release its reference design which will be done using Vivado and IP Integrator. A date of 3/17 was given so we'll see.

    Here's the relevant link at AD's site. You may need to create a dummy account to access it.

    http://ez.analog.com/thread/40069

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer