Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum How to re-route PS-GPIO/MIO to EMIO pin in XPS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1745 views
  • Users 0 members are here
Related

How to re-route PS-GPIO/MIO to EMIO pin in XPS

Former Member
Former Member over 12 years ago

I need to allocate an EMIO pin to be used for the PS GPIO/MIO. What is the process to make this allocation ? where all do the changes need to be made ? It is similar to what has been done in the ZedBoard, just with a different LOC and GPIO pin number. In the ZedBoard, LOC G17 EMIO pin is allocated to PS GPIO 0 and used as a USB PHY reset signal. We need to do something similar, just with a different LOC and GPIO. Please advise.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Chapter 3 of the Zynq Concepts, Tools and Techniques tutorial for the ZedBoard details how to do exactly that. It connects the external BTNR pushbutton input, connected to the PL logic, to the PS GPIO via the EMIO.

     

    http://www.zedboard.org/design/1521/11

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Thanks for the link, I have just one query, is it necessary to add the AXI GPIO core to the design ? Can't the GPIO be directly mapped ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    You can directly map GPIO from the PS or add an AXI GPIO core. The example in chapter 3 of the CTT demonstrates both options. The GPIO connection to the BTNR pushbutton is mapped directly (via EMIO) to the PS GPIO as you would like to do. The BTNU pushbutton is connected to an AXI GPIO core. You don't need to add the AXI GPIO core to use the PS GPIO via the EMIO.

     

    -Gary