Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Flash programming of Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 370 subscribers
  • Views 1122 views
  • Users 0 members are here
Related

Flash programming of Zedboard

nagakiranbj
nagakiranbj over 9 years ago

I am working on Zedboard where it is required for me to store FPGA configuration file(.mcs file) onto Flash.

Zedboard works fine in the JTAG mode. But however FPGA_done LED does not glow if I choose flash method of loading the file.

I am using the following command for converting .bit to .mcs file conversion in Vivado 2014.4:

 write_cfgmem -format mcs -interface spix1 -size 32 -loadbit "up 0x0 c:/main.bit" -file main.mcs

 I also have set JP7 to JP11 jumpers to 00010 for Flash mode.

I find that flash memory gets erased, programmed and verified properly as displayed in Vivado tool.

 Am I missing anything. Please help.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Nagakiranbj,

    Are you following some tutorial or are you trying to load your own custom hardware / application into the QSPI? 

    If you can, please download the 2014.4.1 Developing Zynq Software Speedway. Then install the lab 6 solutions and proceed to do lab 7 of the speeday (or start from lab 1 and work through lab 7). In lab 7 it goes over how to generate a .mcs file and program it into the QSPI. If you still see the same issues as you stated above, you may have an hardware issue that we will investigate next.

    http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-201441-20152-and-20162

    --Josh