Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum FreeRTOS lwIP Echo Server on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 370 subscribers
  • Views 924 views
  • Users 0 members are here
Related

FreeRTOS lwIP Echo Server on Zedboard

e14 Contributor
e14 Contributor over 9 years ago
Hi,
 
I have a  Zedboard and using the Xilinx SDK 2016.1 I have created an application project from the built-in template "FreeRTOS IwIP Echo Server".  This template is found by selecting the freertos823_xilinx as the OS Platform option that the SDK gives you.  This is a rather simple program, described as follows:
 
"The FreeRTOS lwIP Echo Server application provides a simple demonstration of how to use the light-weight IP stack (lwIP) with FreeRTOS. This application sets up the board to use IP address 192.168.1.10, with MAC address 00:0a:35:00:01:02. The server listens for input at port 7 and simply echoes back whatever data is sent to that port."
 
When I deploy on the hardware, I get the following:
   
  -----lwIP Socket Mode Echo server Demo Application ------
  Start PHY autonegotiation 
  ERROR: DHCP request timed out
  Configuring default IP of 192.168.1.10
  Board IP: 192.168.1.10
  Netmask : 255.255.255.0
  Gateway : 192.168.1.1
   
                Server   Port Connect With..
  -------------------- ------ --------------------
           echo server      7 $ telnet <board_ip> 7

 

The application then waits for connections, which I verified by adding some debug statements near the while loop where lwip_accept is executed.  When I use TeraTerm from my Windows 7 host, I get "Connection timed out".   I made sure the connection is to 192.168.1.10, port is 7, and I tried all the available Protocol options TeraTerm provides, and still the connection times out.  I tried to connect using TeraTerm from another computer and get the same result.  Could this be an incompatibility between the IP version of TeraTerm and IwIP?

Thanks.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Swengr16,

    Do you have your ehternet connection set up? I just replicated the application your working with using SDK 2016.2 on a MicroZed. The only time my connection timed out was when I disconnect my ethernet cable. Everytime it was plugged in it worked perfectly.

    --Josh