Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum MicroZed - SDSoC - No Linux TCF Agent running on the specified IP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 371 subscribers
  • Views 1476 views
  • Users 0 members are here
Related

MicroZed - SDSoC - No Linux TCF Agent running on the specified IP

lucileklang
lucileklang over 9 years ago

Hi,

I'm a newbie in using Xilinx tools and Microzed board, and just started to try to set up everything.

I first followed the tutorial "Microzed Getting Started" and set up the Hardware as explained in section 7.1. I also booted the Microzed from the microSD card like in Appendix E.
https://www.avnet.com/opasdata/d120001/medias/docus/4/Avnet-MicroZed-Getting-Started-EN-User-Guide.pdf


I downloaded the SDSoC environment for Windows 10, and tried to achieve the tutorials in SDSoC intro tutorial, and had some problems.

https://www.xilinx.com/support/documentation/sw_manuals/xilinx2016_3/ug1028-sdsoc-intro-tutorial.pdf

On the lab 1, I couldn't run the project on my microzed : the command  /mnt/ lab1.elf answered me " /mnt/ lab1.elf
not fount"
I scrolled in the booting (In SDSoC termnal) to check if something was wrong, and I noticed that I didn't get the line "Starting tcf agent : OK"
Thus I suspected a problem with TCF or booting linux on the SD card.
On the Target Connection windows, I double clicked on "Linux Agent [default]" and changed the IP adress to the IP of the microzed 192.168.1.10 (found with ifconfig). When I clicked on "Test Connection", I got the error "There is no Linux TCF Agent running on the specified '192.168.1.10'"

Maybe the default port 1534 is wrong ? Maybe something's gone wrong when I boot the board ? The SDSoC tutorial is written for a  ZC702 board and not a microzed so maybe some connections are different ?
I'm lost on how to solve this, any help would be greatly appreciated !

Thanks

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello,

    Please try going through the MicroZed Chronicles that target SDSOC (issues 85-93)

    http://zedboard.org/content/microzed-chronicles

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lucileklang
    0 lucileklang over 9 years ago

    Hello,
    Thank you for your link, that enabled me to fix the first part of my problem. But when I follow the instructions on the Chronicle Part 93, to use the debug option, I can get up to creating a new configuration, but cannot choose my system's IP address as a TCF connection because the environment doesn't find it ... 
    Yet when I boot my board I get the message "Starting the tcf agent : OK"


    Do you have a solution to find my IP address and set up the TCF connection ?
    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lucileklang
    0 lucileklang over 9 years ago

    PRECISIONS 

    I checked if I could ping 192.168.1.100 (my board's Ip address) from the command prompt in Windows, yes.
    Yet if I check ifconfig in TeraTerm I don't get the IP adress :
     

    eth0      Link encap:Ethernet  HWaddr 00:0A:35:00:1E:53
              inet6 addr: fe80::20a:35ff:fe00:1e53%767856/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:124 errors:0 dropped:0 overruns:0 frame:0
              TX packets:12 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:9784 (9.5 KiB)  TX bytes:2016 (1.9 KiB)
              Interrupt:144 Base address:0xb000

    Thank you