Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum How to cross compile a downloaded project?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 371 subscribers
  • Views 653 views
  • Users 0 members are here
Related

How to cross compile a downloaded project?

hai.bi
hai.bi over 11 years ago

I downloaded the iwconfig project from hp.  I can compile it in my CentOS using make, but I am thinking that is to run in CentOS. 

What do I need to do so I can get the runtime code so I can copy to my MicroZed SD card to run in Petalinux?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hello hai.bi,

    Is there a specific reason that you are using iwconifg?  If not, you might want to consider switching over to iw instead:

    https://wireless.wiki.kernel.org/en/users/documentation/iw

    We use iw in the Getting Started Guide for our Wilink8 adapter board:

    http://zedboard.org/sites/default/files/documentations/GSG-AES-PMOD-WILINK8-G-v1_6.pdf

    This Xilinx discusses briefly this but you may find it easier to cross-compile with the Zynq toolchain that comes with SDK outside of PetaLinux:

    http://forums.xilinx.com/t5/Embedded-Linux/How-to-add-wireless-tools-to-linux/td-p/440360

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hai.bi
    0 hai.bi over 11 years ago in reply to zedhed

    Thanks Kevin for mentioning iw.  I didn't use it because I didn't realize this replaced iwconfig.  I will give it a try, but I am not familiar with the cross compile either.


    I am working on CentOS host, and I looked at http://wiki.beyondlogic.org/index.php?title=Cross_Compiling_iw_wpa_supplicant_hostapd_rfkill_for_ARM for reference. 


    At first, I used arm-linux-gnueabi as --host param and the make/make install both worked for libnl, but the iw make failed.  So I was thinking maybe I should use arm-Xilinx-linux-gnueabi

    Then I changed libnl ./configure --host=arm-Xilinx-linux-gnueabi --prefix=/usr/arm-xilinx-linux-gnueabi, but the make install fail now.  So what exact should I do to cross compile libnl and iw using CentOS?  Is there anything I need to do to reverse make install first (which may not be using Xilinx compiler)?