Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Vivado custom VHDL/Verilog block
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 370 subscribers
  • Views 581 views
  • Users 0 members are here
Related

Vivado custom VHDL/Verilog block

e14 Contributor
e14 Contributor over 12 years ago

Hi,

In vivado, I would like to create a vhdl block in my design. I know how to create a custom AXI IP, but I didn't find a solution to create a custom VHDL block. Is there a solution to create it ?

Regards,

Snoopy

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Look at the Xilinx Vivado "Design Suite Users Guide - Designing with IP" (UG896) for details: http://www.xilinx.com/support/documentation/sw_manuals/xilinx2014_2/ug896-vivado-ip.pdf

     

    In summary what you will do is open Vivado and select the device (Zynq I assume) that you want to target and either add an existing HDL file or create a new one. Once you are happy with the operation of the HDL block then you can go up to 'Tools' on the Vivado tool bar and select 'Create and Package IP'. Then follow the steps to package your current project as an IP. Once this is complete you will need to add the directory this project is in to a repository visible to your top level project. Then your new custom HDL module will appear as one of the IP selections in the IP Integrator.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Gary,

    Thanks for the response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi

    Am new to Vivado pls can anyone help me to create a custom IP using verilog with an example.

    Regards
    Govind Raj

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The lab material in the Avnet Developing ZynqRegistered-7000 All Programmable SoC Hardware (Vivado 2013.3) Speedway Design seminar includes an example creating custom IP using Verilog. You can download the Speedway material here:

     

    http://zedboard.org/support/trainings-and-videos

     

    -Gary