Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Vivado Read-Only files
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 3109 views
  • Users 0 members are here
Related

Vivado Read-Only files

e14 Contributor
e14 Contributor over 9 years ago

I am using Vivado 2015.2.1 and downloaded FPGA project ccfmc but several source files ie: 'axi_ad9361_rx.v' are Read-only and I am unable to edit it.  I can read and write it in windows but not in the Vivado editor.  I have looked every where I could think of for file properties that will allow editing.  Any help??     

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Wolfejf,

    Could you please reference a link to the project you are talking about?

    What Vivado version is the project targeting? I have seen this error when opening a project that was created in a different Vivado version then the one I was trying it open it with.

    Is Vivado telling you that the some of the IP is out of date and cannot be edited?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    I am using Vivado version 2015.2.1.  I down loaded hdl-2015_r2 and it said to use Vivado version 2015.2.1.  I am using project ccfmc.  No the Vivado IP's are all up to date.  The problem is that several but no all of the source files are Read-only and I can not edit them.  ie: source file "axi_ad9361_rx.v" is a read only file and I can not edit it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    This is a Picozed project targeting development kit AES-PZSDRC-FMC-G down loaded from github.

    Wolfejf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 9 years ago

    I believe this is happening because the verilog file is part of an IP block that is used in the larger IPI design. It's expected behavior for Vivado. It's forcing you to go back to the IP project itself to make modifications.

    /Matt