Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Cannot include .hpp file in Vivado HLS (using OpenCV)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 371 subscribers
  • Views 2543 views
  • Users 0 members are here
Related

Cannot include .hpp file in Vivado HLS (using OpenCV)

e14 Contributor
e14 Contributor over 11 years ago

I want to use OpenCV functions in a project in Vivado HLS. Although I have gone through many tutorials by Xilinx regarding this, I couldn't get how to include these header files so that Vivado HLS (2014.2) detects them.

This is what I have done so far:

I created a project to detect Sobel edges on Visual Studio (2010). My code works well with this (I am using OpenCV version 2.4.9).

I use this same project with Vivado HLS. These are the steps:

I open VivadoHLS, and click on Create New Project. I give a project name as Sobel_Edge (located on C Drive).
Click on Add Files. Browse to the path where I have the Visual Studio Project (in C Drive) and select the EdgeSobel.cpp file. Click on Next.
It then asks for the testbench files. I select the same file (EdgeSobel.cpp) and also select an input image (Img2_g.bmp). Click on Next. Solution Configuration is xq7z020cl1400-2i. Click on OK and Finish.
Now, I click on C Synthesis.

I get an error saying core.hpp is not found, although it is present in the location: E:XilinxVivado_HLS2014.2includeopencv2core.

When I type the entire location of core.hpp as:

#include <E:/Xilinx/Vivado_HLS/2014.2/include/opencv2/core/core.hpp>

then this file, core.hpp is detected but types_c.h will not be detected, since it'll only be

#include "opencv2/core/types_c.h"
Here too, when I give the entire path as mentioned below, the error goes and the next file will not be detected.

#include "E:/Xilinx/Vivado_HLS/2014.2/include/opencv2/core/types_c.h"
So basically, it expects me to give the entire path of where the file is located in all lines within the header files. Is there a way by which I can set the directory, so that it looks in the same path always?

What are the settings I have to make?

Let me know if any other information is required to help me solve this issue.

Regards.

  • Sign in to reply
  • Cancel
  • kotrasharmila
    0 kotrasharmila over 7 years ago

    hi,

    i also got the same error anyone please hep me out..

    thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago

    Hello,

    Please post this question over at the Xilinx support forum.
     

    Thank you,

    Josh