Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Vivado And SDK on Ubuntu 14.04.2 LTS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 370 subscribers
  • Views 647 views
  • Users 0 members are here
Related

Vivado And SDK on Ubuntu 14.04.2 LTS

e14 Contributor
e14 Contributor over 10 years ago

Hi

I just installed Vivado 2015.1 with SDK using the Web installer on UBUNTU 14.04.2 LTS 64bits running on a VMware workstation with windows 7 as host operating system.

I've been working with Vivado releases on Windows without anyproblem but on UBUTNU I can't even run a simple hello world project, it seems there is a problem with compiler settings. this are the errors I get in the console and so far haven't managed to solve:

10:44:30 **** Build of configuration Debug for project hello_world ****
make all
Building file: ../src/helloworld.c
Invoking: ARM gcc compiler
arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MT"src/helloworld.o" -I../../hello_world_bsp/ps7_cortexa9_0/include -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o "src/helloworld.o" "../src/helloworld.c"
Finished building: ../src/helloworld.c

Building file: ../src/platform.c
Invoking: ARM gcc compiler
arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MT"src/platform.o" -I../../hello_world_bsp/ps7_cortexa9_0/include -MMD -MP -MF"src/platform.d" -MT"src/platform.d" -o "src/platform.o" "../src/platform.c"
Finished building: ../src/platform.c

Building target: hello_world.elf
Invoking: ARM gcc linker
arm-xilinx-eabi-gcc -Wl,-T -Wl,../src/lscript.ld -L../../hello_world_bsp/ps7_cortexa9_0/lib -o "hello_world.elf"  ./src/helloworld.o ./src/platform.o   -Wl,--start-group,-lxil,-lgcc,-lc,--end-group
/opt/Xilinx/SDK/2015.1/gnu/arm/lin/bin/../lib/gcc/arm-xilinx-eabi/4.9.1/../../../../arm-xilinx-eabi/bin/ld: warning: cannot find entry symbol _vector_table; defaulting to 00000000
./src/helloworld.o: In function `main':
/home/sebastian/Dev/xilinx/hm/hm.sdk/hello_world/Debug/../src/helloworld.c:57: undefined reference to `print'
./src/platform.o: In function `disable_caches':
/home/sebastian/Dev/xilinx/hm/hm.sdk/hello_world/Debug/../src/platform.c:69: undefined reference to `Xil_DCacheDisable'
/home/sebastian/Dev/xilinx/hm/hm.sdk/hello_world/Debug/../src/platform.c:70: undefined reference to `Xil_ICacheDisable'
collect2: error: ld returned 1 exit status
make: *** [hello_world.elf] Error 1

10:44:31 Build Finished (took 619ms)

I've read that it might be due to lack of 32bits libraries which I installed and tried  but this erors do not go, I would appreciate if anyone knows how to solve this problem.

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Have you looked at Sven Andersson's blog: http://svenand.blogdrive.com/
     
    He has been successfully using PetaLinux under Ubuntu 14.04 so you might want to see if his blog might be helpful.
     
    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I came back to Vivado and set zynq system to Zedboard preset, exported the hardware again, back in SDK created a new stand alone application with a hello world template and compiled it without any problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    In order to start developing applications, you must install the Platform-tools and at least one version of the Android platform, using the SDK Manager. Platform-tools contains build tools that are periodically updated to support new features in the Android platform which is why they are separate from basic SDK tools including adb dexdump and others.http://www.pass4sureexam.co/vendor/VMware