Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum ILA and Vivado via Petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 370 subscribers
  • Views 1267 views
  • Users 0 members are here
Related

ILA and Vivado via Petalinux

e14 Contributor
e14 Contributor over 10 years ago

I'd like to use the Vivado Integrated Logic Analyzer (ILA) and connect to it over the network.  Additionally, I'd like this connection to be made via the PS on the same Zynq chip as the PL being monitored.

It looks like Vivado can be pointed at a network device for the connection.  See http://www.xilinx.com/support/documentation/application_notes/xapp1251-xvc-zynq-petalinux.pdf. However, that app note requires a second board and looks to me like just a way of building a network dongle instead of using the USB dongle sold by Xilinx.  I'd like a solution that doesn't require managing an additional board/piece of hardware.

I've found a related (though possibly more general) question at https://forums.xilinx.com/t5/7-Series-FPGAs/Is-it-possible-to-control-PL-JTAG-from-PS-in-the-same-Zynq-FPGA/td-p/672775, which suggests that it's not possible to do what I'm after given that the ILA is controlled via JTAG.

Is there another variant of the ILA (or configuration option) so that the ILA can be accessed over the AXI bus instead of over the JTAG?  Is there another tool that I haven't found yet that does what I'm looking for?

Thanks,

Tom

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Tom,

     

    Your second link is broken but I was able to find the post with a search.

    https://forums.xilinx.com/t5/7-Series-FPGAs/Is-it-possible-to-control-PL-JTAG-from-PS-in-the-same-Zynq-FPGA/m-p/672775#M14513

     

    This is a good question. I don't know the answer for sure, but it post implies that you might be able to do this with an external connection from the AXI-JTAG signals back to the Zynq JTAG inputs. Probably a better question to follow up with on the Xilinx forums. Let us know if you do find out more on this method.

     

    The only other related post I could fine is this one: http://zedboard.org/content/jtag-axi-and-ila-issues

     

    If any of our other forum users have done something like this please let us know how it worked.

     

    -Gary