Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum No spi node found in /dev folder
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 370 subscribers
  • Views 661 views
  • Users 0 members are here
Related

No spi node found in /dev folder

e14 Contributor
e14 Contributor over 10 years ago

Hello everyone

I am using ubuntu 14.04 ,vivado 2015.2 and petalinux.BSP 2015.2 version and working for Xilinx Zedboard 7z020

I want to send /receive data from Spi, I created my project and generate the .hdf and .bit file after that export it to SDK


then I create a project using defined BSP

$petalinux-create -t project -s /Downloads/Avnet-2015.2.BSP


get the hardware

$ petalinux-config --get-hw-description=~/my_program/my_program.sdk


run petalinux configuration

$petalinux-config

subsystem Auto hardware setting->Advance bootable image storage setting and select sd-card for boot image ,kernel image and dtb image setting

in the system-top.dts I add the following lines

&spi0 {
is-decoded-cs = <0>;
num-cs = <3>;
status = "okay";
  spidev@0x01 {
        compatible = "spidev2";
        spi-max-frequency = <20000000>;
        reg = <1>;
    };
};
&spi1 {
is-decoded-cs = <0>;
num-cs = <3>;
status = "okay";
spidev@0x00 {
        compatible = "spidev1";
        spi-max-frequency = <20000000>;
        reg = <1>;
    };
};


build the images

$petalinux-build


generate BOOT.BIN:

$petalinux-package --boot --format BIN --fsbl ~/Avnet-Digilent-ZedBoard-2015.2/images/linux/zynq_fsbl.elf --fpga ~my_program/my_program.sdk/system_wrapper_hw_platform_0/system_wrapper.bit --u-boot

generate rootfs.cpio with the following command because I want to boot the board with sd-card


$petalinux-package --image -c rootfs --format initramfs


IN the sd card copy BOOT.BIN , image.ub and system.dtb into BOOT partition and rootfs.cpio into rootfs partition then run the following command


$sudo pax -rvf rootfs.cpio


In the last boot the board with this sd card

and the result is, I cannot find any /dev/spidev


even whatever changes I made in the sytem-top.dts after running the above commands these changes has been removed and the file name is system.dts, I also checked result is same if i am not adding the above defined lines in the system-top.dts

can anyone help me where i am doing mistake ??/

One more thing I want to check that is this kernel is working or not , I run the following commands

$ cd /sys/class/gpio

/sys/class/gpio$ echo 61>export

but no node generated for GPIO

that means it is also not working

what mistake I am doing??

thanks in advance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Umer,

     

    I see that you received a response to this question that you posted on the Xilinx Community Forums:

     

    https://forums.xilinx.com/t5/Embedded-Linux/petalinux-not-generate-the-required-spidev/td-p/670901

     

    If you do cross post questions on other forums, and get an answer, please pass that along so that others on the forum can benefit as well.

     

    -Gary