Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard CTT and IOSTANDARD and LOC problems.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 353 subscribers
  • Views 807 views
  • Users 0 members are here
Related

Zedboard CTT and IOSTANDARD and LOC problems.

Former Member
Former Member over 12 years ago

I'm going thru Zedboard_CTT_v2013_2_120807 tutorial using Vivado2013.4 and I'm stuck at 5.4 - Controlling LED's and Switches in Linux example.

I built a design and ran thru Synthesis and Implementations successfully, but failed to generate bitstream with 2 errors:
1 - [Drc 23-20] Rule violation (NSTD-1) Unspecified I/O Standard - 21 out of 151 logical ports use I/O standard (IOSTANDARD) value 'DEFAULT', instead of a user assigned specific value...
2 - [Drc 23-20] Rule violation (UCIO-1) Unconstrained Logical Port - 21 out of 151 logical ports have no user assigned specific location constraint (LOC).


Am I missing something?


I googled the topic and looks like I have to add constraints like it mentioned here: http://zedboard.org/content/ise-146-missing-leds8bits-btns5bits-sws8bits


But... First, why it is not mentioned in a tutorial? Second, looks like LED's and Buttons conneted to 3.3V and Switches can be selected by VADJ on Zedboard(on my 3V3 jumper not even populated, so its either 1.8V or 2.5V) and in a post above it suggested to specify 3.3 for all pins. So, I got a little confused and really don't want to damage the board.


Also, in CCT offset address for leds_8bits, btns_5bit and switched_8bit differ from "Basic Vivado IPI Design" example. Why? Which one correct and how/where I can find out the correct offsets without asking here?


Can anybody clarify situation. Thank you in advance.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Confirmed.

    I'm positive I did use "Preset" in a step6, but after recreated design one more time I was able to generate "bitstream" without manually settings constrains. Idk what went wrong.

    I guess in a future I will go twice thru each step :)

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Confirmed.

    I'm positive I did use "Preset" in a step6, but after recreated design one more time I was able to generate "bitstream" without manually settings constrains. Idk what went wrong.

    I guess in a future I will go twice thru each step :)

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    i'm not sure but this might help some people,
    i ran into the same sort of problems while i was following different tutorials,
    be careful when you start creating a new project and creating a new h/w specification, when you call for the board template you are using, it may propose different kind of basic IO featured on the board.
    For instance i use the zedboard and the template loads an XML which says that we have 5 BTNS, 8 SWs, 8LEDS on the programmable logic.

    But when you want to start interacting with these, you have to specify a LOC in an UCF file.
    If you called the template, netting inside the ucf file will lead to a conflict.

    I prefer removing any IO and starting with the naked board. Then i create a proper ucf file for every .bitstream made of every single net that i need.