Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Another Usefull Reference Projects
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 693 views
  • Users 0 members are here
Related

Another Usefull Reference Projects

Former Member
Former Member over 13 years ago

There is a nice project:
http://zynqgeek.blogspot.com/2012/09/creating-custom-peripheral.html

But how can I use this port (register) assigned to external pins? For example, write to the LEDs and read the switches.

And how can I write my independent HDL code, for example, just reflect on LED0 (LD0) the state of the switch0 (SW0).

I'm used to FPGAs and the ISE environment, but I'm having some trouble trying to do these simple tasks with the Zynq.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    Hello,

    When I tried to use LEDs with my custom peripheral, I had troubles with constraints: the ports I added were not recognized.
    Here is what I do to make it work:
    - I change user_logic.vhd and top level zed_leds.vhd => my new ports are "LEDS : out std_logic_vector(7 downto 0);"
    - in XPS, I add my custom peripheral named zed_leds
    - in XPS, in "ports" tab, at zed_leds line, my ports are not visible...
    - close XPS and change zed_leds_v2_1_0.mpd (zed_leds_pl.srcssources_1edkproc_modulepcoreszed_leds_v1_00_adata) => add "PORT LEDS = "", DIR = O, VEC = [7:0]" in "PORTS" section
    - save and relaunch XPS => in "ports" tab, LEDS is now visible!
    - connect to "External Ports::zed_leds0_LEDS_pin"
    - exit XPS
    - create .ucf file => "NET zed_leds_0_LEDS_pin[0] IOSTANDARD=LVCMOS25 | LOC=T22;" for led0, and so on.
    - enjoy

    I am not sure this is the right way but, well, if it can help...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    Hello,

    When I tried to use LEDs with my custom peripheral, I had troubles with constraints: the ports I added were not recognized.
    Here is what I do to make it work:
    - I change user_logic.vhd and top level zed_leds.vhd => my new ports are "LEDS : out std_logic_vector(7 downto 0);"
    - in XPS, I add my custom peripheral named zed_leds
    - in XPS, in "ports" tab, at zed_leds line, my ports are not visible...
    - close XPS and change zed_leds_v2_1_0.mpd (zed_leds_pl.srcssources_1edkproc_modulepcoreszed_leds_v1_00_adata) => add "PORT LEDS = "", DIR = O, VEC = [7:0]" in "PORTS" section
    - save and relaunch XPS => in "ports" tab, LEDS is now visible!
    - connect to "External Ports::zed_leds0_LEDS_pin"
    - exit XPS
    - create .ucf file => "NET zed_leds_0_LEDS_pin[0] IOSTANDARD=LVCMOS25 | LOC=T22;" for led0, and so on.
    - enjoy

    I am not sure this is the right way but, well, if it can help...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data