Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard DDR3 interface address space?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 626 views
  • Users 0 members are here
Related

ZedBoard DDR3 interface address space?

Former Member
Former Member over 12 years ago

Hi,
According to ZedBoard user guide, The multi-protocol DDR memory controller is configured for 32-bit wide accesses to a 512 MB address space.

But I was wondering, how would I be able to target only ONE of the Micron MT41K128M16HA-15E components?

In other words, for my specific application, I have two VDMAs that are streaming to DDR. But I would prefer to know that the data from one VDMA is streamed into only one of the Micron memory components, and my data from the second VDMA targets ONLY the second memory component!!

Thanks in advance,
--Rudy


  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Bryan,
    Thanks for the reply. But, is this how usually what happens when you write a 32-bit wide data into a two sets of 16-bit wide memory?

    Is that right that the first 16-bit gets stored in one RAM, and the other 16-bit gets stored in the second RAM?

    Because if this is the case, I can do this for my application, since in this specific application I don't really care about what I am writing into the DDRs !!

    But how do I know this is how the data is getting managed in the DDRs?
    Why not Byte-0 and Byte-1 getting stored in one DDR, and Byte-2 & Byte-3 is also in the subsequent address of the same DDR ?!
    I am sorry that if this is an obvious question, but I just didn't know how the 32-bit data is stored in two 16-bit SDRAM !
    Is this true for all sorts of board, which uses SDRAMs in parallel, or is this only true for the ZedBoard case?

    Thanks,
    --Rudy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago in reply to Former Member

    Rudy,

    Yes, that is definitely the case here. The ZedBoard was designed to have a 32-bit wide interface between the memory and the Zynq. The schematic and layout connect the configuration with bits 0 through 15 going to one chip and 16 through 31 going to another. This is the fastest, most efficient way. For every 32-bit word that you read or write, 1/2 is associated with one chip and 1/2 with the other.

     

    I believe this would be the case for every 32-bit processor that you see with 2 x16 chips attached to it.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago in reply to Former Member

    Rudy,

    Yes, that is definitely the case here. The ZedBoard was designed to have a 32-bit wide interface between the memory and the Zynq. The schematic and layout connect the configuration with bits 0 through 15 going to one chip and 16 through 31 going to another. This is the fastest, most efficient way. For every 32-bit word that you read or write, 1/2 is associated with one chip and 1/2 with the other.

     

    I believe this would be the case for every 32-bit processor that you see with 2 x16 chips attached to it.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data