Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 'No Load' Parts in the ZedBoard schematics
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 957 views
  • Users 0 members are here
Related

'No Load' Parts in the ZedBoard schematics

e14 Contributor
e14 Contributor over 13 years ago

In the ZedBoard schematics, several parts are marked with 'No Load' and some resistors have a 0 u2126 value. I want to copy and modify the schematics for my design. What is the best way to handle these alternative hardware features?
Has anyone already found out what is the best solution? Is it the best way to omit the 'No Load' parts and replace the 0 u2126 resistors by a wire?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    All of our existing designs and hardware guide publish results for the default configuration.  In that case, you can ignore all No-Load parts, replace 0-ohm resistors with wires, and replace jumpers with wires for your preferred configuration.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    All of our existing designs and hardware guide publish results for the default configuration.  In that case, you can ignore all No-Load parts, replace 0-ohm resistors with wires, and replace jumpers with wires for your preferred configuration.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Hi Bryan,
    Thank you - I have done this. I found one problem: the signal SPI-SCLK-FB/VCFG1 is pulled up (R177 - 20 ku2126 to 3,3V) but has no connection. Does it have any sense?
    Bahne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    SPI-SCLK-FB/VCFG1 is tied to MIO8 on the Zynq device.  This pin has 2 purposes. 

    1.   Voltage Mode Setting (see Zynq TRM v1.5, page 146).  MIO8 is VMODE[1].  Pulling this up sets the MIO Bank 1 I/O Voltage to 1.8V.
    2.   Quad-SPI Feedback Clock (see Zynq TRM v1.5, page 307).  The Quad-SPI interface supports an optional feedback clock pin named qspi_sclk_fb_out. This pin is used with the high speed Quad-SPI timing mode, where the memory interface clock needs to be greater than 40 MHz.  When Quad-SPI feedback mode is used, the qspi_sclk_fb_out pin should only be connected to a pull-up or pull-down resistor which is needed to set the MIO voltage mode (vmode).

    Bryan