Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design BIST (built in self test)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 345 subscribers
  • Views 484 views
  • Users 0 members are here
Related

BIST (built in self test)

Former Member
Former Member over 10 years ago

Hi people,

  Sorry for asking what seems to be a silly question, but I couldn't find in the documentation nor in other forums. I am having a problem with the integration of my zedboard and a board from Analog Devices... and it seems I have a problem with one specific zedboard, because it works with other zedboards.... I was wandering if the zedboard has a BIST mode. 


  It seems BIST is available for some of the Xilinx boards (http://www.xilinx.com/support/documentation/boards_and_kits/UG926_Z7_ZC702_Eval_Kit.pdf, page 13) , but I dind't manage to find the an equivalent for for the zedboard.


  Anyone has an idea how could I see if the board has an specific problem? Both boards seems to work perfectly, I manage to boot, to use the programable logic, etc. Both are the same review (REV C) the jumpers are put the same way, the hard log from the hardware manager is exactly the same... but in one zedboard my analog device board works perfectly in the other no!


  Thanks in advance...


        Daniel

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    There is not Built in Self Test on the ZedBoard.

     

    As a substitute you might want to generate the peripheral and memory tests from the built in SDK templates. Lab 4 fo the Avnet Zynq SW Speedway training material steps you through how to generate and run these tests. It also shows you how to modify the memory test to check the complete DRAM memory.

     

    The Speedway lab files can be downloaded here: http://picozed.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    There is not Built in Self Test on the ZedBoard.

     

    As a substitute you might want to generate the peripheral and memory tests from the built in SDK templates. Lab 4 fo the Avnet Zynq SW Speedway training material steps you through how to generate and run these tests. It also shows you how to modify the memory test to check the complete DRAM memory.

     

    The Speedway lab files can be downloaded here: http://picozed.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441

     

    -Gary