Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design CDMA PS to PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 388 views
  • Users 0 members are here
Related

CDMA PS to PL

Former Member
Former Member over 12 years ago

Hi

I tried to add two inputs and save the result into shift reg.
If shift reg is full, then I want "CDMA" between shift reg and DDR3.

So, I added GPIO for external port to connect this port with "adder"
Then, I connected to shift register
Also, in XPS I used CDMA tutorial design (CDMA tutorial UG873 == DDR3 --> DDR3 data transfer).

GP0 -- interconnect -- GPIO         ---- ADDER --- shift_reg
HP0 & HP2 --interconnect --CDMA
---------------------------         ------------------------
----------PS----------------       ------------PL-----------


However, I got error about constraint .UCF
which is

/////////////////////////////////////////////////////////////

ERROR:Bitgen:342 - This design contains pins which have locations (LOC) that are
   not user-assigned or I/O Standards (IOSTANDARD) that are not user-assigned.
   This may cause I/O contention or incompatibility with the board power or
   connectivity affecting performance, signal integrity or in extreme cases
   cause damage to the device or the components to which it is connected.  To
   prevent this error, it is highly suggested to specify all pin locations and
   I/O standards to avoid potential contention or conflicts and allow proper
   bitstream creation.  To demote this error to a warning and allow bitstream
   creation with unspecified I/O location or standards, you may apply the
   following bitgen switch: -g UnconstrainedPins:Allow

//////////////////////////////////////////////////////////////


I don't know how to fix it...(Also, I am not sure my thought is right choice or not)
it seems that somehow I have to make constraint file.
Can someone help me to make .UCF file?
or is there better idea to design for my purpose?




Second, I got fft ip(belfft) from this website. it generates own IP. I am trying to add this IP in PS level (in XPS).
when I try to synthesize and bit generate, it didn't show any errors.

So, I want to add this FFT IP in CDMA design in XPS.


this is original CDMA tutorial example

M_GP0 --- interconnect_gp --- S_CDMA_M ----interconnect_hp -- S_HP0 & S_HP2 ---- DDR3


and this is my expected design.
(FFT --> save into BRAM --> interrupt @ CDMA --> BRAM to DDR3)

which position do I need to consider for FFT IP, BRAM controller, and BRAM?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    If someone can help me, I can send you picture so that it may help to understand the problem clearly
    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    If someone can help me, I can send you picture so that it may help to understand the problem clearly
    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data