Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AXI VDMA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 1443 views
  • Users 0 members are here
Related

AXI VDMA

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am having a problem with a simple design on the zedboard. My design consists of a Zynq processor, AXI VDMA, and a AXI TPG. The axi stream clock is set to run at 150Mhz (142.85Mhz actual). The problem is when I synthesize the design it fails timing. The AXI VDMA product guide PG020 shows that the Artix-7 family -1 speed grade can do 150 MHz AXI4-stream.

These are links of images for the timing report.
postimg.org/image/mx3xzenji
postimg.org/image/c206c42p3

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 12 years ago

    Looking all that over, nothing looks out of place. 
    I'm not sure I see where Artix-7 is mentioned in PG020, you are right though, that Zynq can do a 64bit AXI connection at 150Mhz (MAX).

    I still believe that you need to change the constraint that is there.  If you did not have any constraints, it would just pass timing.  Since you did not add any, this must be part of the auto-generated constraints.  Files are called *.xdc and are located in the project folder.

    Again, I suggest you look at your clock tree and modify it to get 150Mhz, if that is what you NEED.  If the constraint is for 150Mhz, and you are getting 142Mhz, you are most likely out of tolerance in the constraint's eyes.  Thus you fail either setup or hold.

    Probably the easiest thing to do, is change the 150Mhz to something else that is a better multiple.  If you do not need it, why push the fabric?  It is only going to make routing difficult as well as consume more power.

    If you NEED 150Mhz, I suggest you disable the 150Mhz FCLK, then in the BD, add a MCMM.  Then use the MCMM to create the 150Mhz.  Using the MCMM IP allows you to choose MCMM or PLL.  UG472 suggests you use a MCMM, unless you need extra jitter control or cannot make the clock frequency that you need.  At 150Mhz, you should start to be concerned with jitter, so my guidance is use the PLL suggestion, if it will give you 150Mhz.

    From the images, it looks like you are doing 1080P video?  You might want to look at our video Reference designs.  There might be something else that you or I am missing - based on the information you presented to me.
    http://zedboard.org/design/1521/11
    Based on what you told me, I think that this Design might be of some use:
    "Zedboard HDMI Display Controller Tutorial for Vivado"

    Using the information you provided, I come up with needing about a 50Mhz clock.
    Your configuration is:
    (1080*1920)*(24 (RGB))*30(FPS)? = 1,492,992,000 bits/sec
    =186,624,000 Bytes/sec

    So, you really only need to run (at 32bit wide, based on his VDMA block) 46+change Mhz.  So, 50Mhz seems adequate.
    32 bits = 4 bytes
    186624000/4 = 46,656,000/sec (or Hz).

    I'm told that if you are doing 1080P60-FPS, you will need at LEAST a 142Mhz clock, as the pixels rate ends up being 148.5Mhz, however there are blanking periods that allows your 142Mhz clock to catch up to the required 148.5Mhz.

    Did that explanation make sense to you?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 12 years ago

    Looking all that over, nothing looks out of place. 
    I'm not sure I see where Artix-7 is mentioned in PG020, you are right though, that Zynq can do a 64bit AXI connection at 150Mhz (MAX).

    I still believe that you need to change the constraint that is there.  If you did not have any constraints, it would just pass timing.  Since you did not add any, this must be part of the auto-generated constraints.  Files are called *.xdc and are located in the project folder.

    Again, I suggest you look at your clock tree and modify it to get 150Mhz, if that is what you NEED.  If the constraint is for 150Mhz, and you are getting 142Mhz, you are most likely out of tolerance in the constraint's eyes.  Thus you fail either setup or hold.

    Probably the easiest thing to do, is change the 150Mhz to something else that is a better multiple.  If you do not need it, why push the fabric?  It is only going to make routing difficult as well as consume more power.

    If you NEED 150Mhz, I suggest you disable the 150Mhz FCLK, then in the BD, add a MCMM.  Then use the MCMM to create the 150Mhz.  Using the MCMM IP allows you to choose MCMM or PLL.  UG472 suggests you use a MCMM, unless you need extra jitter control or cannot make the clock frequency that you need.  At 150Mhz, you should start to be concerned with jitter, so my guidance is use the PLL suggestion, if it will give you 150Mhz.

    From the images, it looks like you are doing 1080P video?  You might want to look at our video Reference designs.  There might be something else that you or I am missing - based on the information you presented to me.
    http://zedboard.org/design/1521/11
    Based on what you told me, I think that this Design might be of some use:
    "Zedboard HDMI Display Controller Tutorial for Vivado"

    Using the information you provided, I come up with needing about a 50Mhz clock.
    Your configuration is:
    (1080*1920)*(24 (RGB))*30(FPS)? = 1,492,992,000 bits/sec
    =186,624,000 Bytes/sec

    So, you really only need to run (at 32bit wide, based on his VDMA block) 46+change Mhz.  So, 50Mhz seems adequate.
    32 bits = 4 bytes
    186624000/4 = 46,656,000/sec (or Hz).

    I'm told that if you are doing 1080P60-FPS, you will need at LEAST a 142Mhz clock, as the pixels rate ends up being 148.5Mhz, however there are blanking periods that allows your 142Mhz clock to catch up to the required 148.5Mhz.

    Did that explanation make sense to you?

    --Dan