Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Not detecting eth0 gigabit ethernet
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 352 subscribers
  • Views 244 views
  • Users 0 members are here
Related

Not detecting eth0 gigabit ethernet

Former Member
Former Member over 11 years ago

I am using Zedboard and design given on this blog:

http://shakithweblog.blogspot.kr/2012/12/getting-sobel-filter-application.html

after this I had to run an application which takes the camera frames from eth0

but when I am running ifconfig command it only shows this:
lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:8 errors:0 dropped:0 overruns:0 frame:0
          TX packets:8 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:592 (592.0 B)  TX bytes:592 (592.0 B) 

I guess its the internal loop only it's not showing about the eth0 thats why in my application I am not able to get any camera frames.

Please tel me how can I resolve this ?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    I suggest you use one of the reference designs on zedboard.org and make sure your ethernet/cable/PC setup is working properly. Then compare that design to the blog design. If you still can't figure it out, you might want to contact the owner of the blog.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago

    I suggest you use one of the reference designs on zedboard.org and make sure your ethernet/cable/PC setup is working properly. Then compare that design to the blog design. If you still can't figure it out, you might want to contact the owner of the blog.

    Bryan