Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Communicate with PL from LINUX on PS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 560 views
  • Users 0 members are here
Related

Communicate with PL from LINUX on PS

deaxman
deaxman over 12 years ago

When I try to program the FPGA with the hardware session in Vivado 2013, in the beginning the "diligent" logo will be on and the done light will be on. In this state I can access a serial connection to the board through tera term. As soon as I program it however, the "diligent" logo disapears and I cannot open a serial connection. All I want to do is program the board and then use the linux on the arm processor to read the values for each of the IO, why does programming the PL reset or disable the PS. Thanks a ton to whoever answers this, I'm at a loss.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    The PS can be run independently of the PL. However, the build that ships with the ZedBoard has intertwined the two (OLED and HDMI are both on the PL, but controlled from the PS). If you want to change what is in the PL, you have to be careful with what the PS is doing. You might be better off going with a simpler version of Linux on the PS side. You can take a look at the Intro and Linux trainings here on zedboard.org to see examples of the PS running independent of the PL, and then how to add IP and applications in the PL that interact with the PS.

     

    http://www.zedboard.org/trainings-and-videos

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    The PS can be run independently of the PL. However, the build that ships with the ZedBoard has intertwined the two (OLED and HDMI are both on the PL, but controlled from the PS). If you want to change what is in the PL, you have to be careful with what the PS is doing. You might be better off going with a simpler version of Linux on the PS side. You can take a look at the Intro and Linux trainings here on zedboard.org to see examples of the PS running independent of the PL, and then how to add IP and applications in the PL that interact with the PS.

     

    http://www.zedboard.org/trainings-and-videos

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data