Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Communicate with PL from LINUX on PS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 558 views
  • Users 0 members are here
Related

Communicate with PL from LINUX on PS

deaxman
deaxman over 12 years ago

When I try to program the FPGA with the hardware session in Vivado 2013, in the beginning the "diligent" logo will be on and the done light will be on. In this state I can access a serial connection to the board through tera term. As soon as I program it however, the "diligent" logo disapears and I cannot open a serial connection. All I want to do is program the board and then use the linux on the arm processor to read the values for each of the IO, why does programming the PL reset or disable the PS. Thanks a ton to whoever answers this, I'm at a loss.

  • Sign in to reply
  • Cancel
Parents
  • deaxman
    0 deaxman over 12 years ago

    I have tried setting up microblaze if that's what you mean to support the PS with the PL, is there any documentation you can recommend to this effect?  Ideally I would love to run the Linux that is on the SD card and load a bit file that only changes how the PL responds.  I mainly just want to use linux to moniter the state of the IO and switches LEDs etc while the FPGA is doing whatever is specified by the Bit file.  It seems like you should be able to run them completely independently because it is possible to load a bit file from linux (I know this from the documentation only, I haven't tried it yet) and if that were the case then using linux to load certain bit files would cause linux to crash which seems counter intuitive.  Thanks a ton for the quick response, sorry it took me so long to reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deaxman
    0 deaxman over 12 years ago

    I have tried setting up microblaze if that's what you mean to support the PS with the PL, is there any documentation you can recommend to this effect?  Ideally I would love to run the Linux that is on the SD card and load a bit file that only changes how the PL responds.  I mainly just want to use linux to moniter the state of the IO and switches LEDs etc while the FPGA is doing whatever is specified by the Bit file.  It seems like you should be able to run them completely independently because it is possible to load a bit file from linux (I know this from the documentation only, I haven't tried it yet) and if that were the case then using linux to load certain bit files would cause linux to crash which seems counter intuitive.  Thanks a ton for the quick response, sorry it took me so long to reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data