Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Use only 16 Bit DDR Data Width on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1579 views
  • Users 0 members are here
Related

Use only 16 Bit DDR Data Width on Zedboard

Former Member
Former Member over 12 years ago

Hello everyone,

Zedboard uses two DDR3-SDRAM chip with a width of 16-Data Bits each. So there is a 32 Bit/566 MHz DDR3 interface with a good performance - no doubt about that.

For my application it is maybe sufficient to use only one DDR chip with 16 Bit databus. But I first want to evaluate the performance on the Zedboard.

Ist it posssible to use only one of the DDR memory chips on Zedboard?
Of course I can configure the memory controller in Vivado to use a 16 Bit Databus, but are there any hardware restrictions for my approach on Zedboard?

Regards,
SAT

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    You can configure the ZedBoard to use a 16 bit data bus for the DDR memory. The only impact should be performance.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    If the memories are of 16 bit data each, then while reading or writing from the memory why should we write only to the alternate locations [using xilinx sdk]?.

    Also, are there any locations within the DDR memory which should not written?? Because, when i tried to certain locations and read them back, I was getting back '0' instead of the actual value written

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Where did you see a reference to only writing alternate locations?

     

    Which locations in DDR memory did you have problems writing/reading?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Actually i was facing problems writing 16 bits to memory using the function Xil_Out16. While reading i was not getting the actual valie written to the memory. So, I wrote to alternate locations and then read from them. Then it was working fine.

    I am not sure if this is correct..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Will we be able to write to the entire DDR memory?? Or are there any regions which are reserved?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    You can access DDR memory starting with location 0x00100000 to the 'top' of DDR memory space. The addresses from, 0x00000000 to 0x0000FFFF  are overlaid with the OCM (On Chip Memory).

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    I tried that..
    Started writing from 0x00100000 to 0x0000FFFF.

    But, the console was printing the details of FSBL and other details instead of reading the required values..

    What would be cause of this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer