Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Use only 16 Bit DDR Data Width on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1584 views
  • Users 0 members are here
Related

Use only 16 Bit DDR Data Width on Zedboard

Former Member
Former Member over 12 years ago

Hello everyone,

Zedboard uses two DDR3-SDRAM chip with a width of 16-Data Bits each. So there is a 32 Bit/566 MHz DDR3 interface with a good performance - no doubt about that.

For my application it is maybe sufficient to use only one DDR chip with 16 Bit databus. But I first want to evaluate the performance on the Zedboard.

Ist it posssible to use only one of the DDR memory chips on Zedboard?
Of course I can configure the memory controller in Vivado to use a 16 Bit Databus, but are there any hardware restrictions for my approach on Zedboard?

Regards,
SAT

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    If the memories are of 16 bit data each, then while reading or writing from the memory why should we write only to the alternate locations [using xilinx sdk]?.

    Also, are there any locations within the DDR memory which should not written?? Because, when i tried to certain locations and read them back, I was getting back '0' instead of the actual value written

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    If the memories are of 16 bit data each, then while reading or writing from the memory why should we write only to the alternate locations [using xilinx sdk]?.

    Also, are there any locations within the DDR memory which should not written?? Because, when i tried to certain locations and read them back, I was getting back '0' instead of the actual value written

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data