Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interface 2 zedboards through SPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 2106 views
  • Users 0 members are here
Related

Interface 2 zedboards through SPI

e14 Contributor
e14 Contributor over 10 years ago

Hello guys,
I want to interface 2 zedboards with spi connection with 1 zedboard acting as master and other acting as slave.
I do not how to proceed for this as I did not find any tutorials for the same.
If you have any tutorials for the same, do suggest me.

In the vivado hardware design, I have enabled SPI 1 and mio pins are allocated to mosi,miso,sclk,ss.
How should I make one zedboard as master and other as slave ?
Kindly suggest how to proceed.

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1 verified
    Hello Darpan, Once you have made the physical connections between the boards I would suggest looking at the SPI coding examples included with the SDK. You can access these either via the SDK using the…
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Darpan,

     

    Once you have made the physical connections between the boards I would suggest looking at the SPI coding examples included with the SDK. You can access these either via the SDK using the links on the system.mss or directly, within the Xilinx SDK installation directories.

     

    The AXI SPI examples can be found here in a typical 2015.2 SDK installation:

     

    C:\Xilinx\SDK\2015.2\data\embeddedsw\XilinxProcessorIPLib\drivers\spi_v4_1\examples

     

    The PS SPI examples here:

     

     C:\Xilinx\SDK\2015.2\data\embeddedsw\XilinxProcessorIPLib\drivers\spips_v3_0\examples

     

    I have found the QUAD_AXI_SPI core to be easier to use than the PS based SP controller, but either should work for your application.

     

    -Gary

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks Gary for the help.
    It works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DJK
    0 DJK over 4 years ago in reply to e14 Contributor

    Hello, 

    I’m trying to do the same application but I didn’t find anything in the examples … which example did you use exactly ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 4 years ago in reply to DJK

    Hi DJK,

    You are probably best off asking any questions specific to Zedboard at the Digilent support forum as they are the primary support path for this product. For me I find all the driver specific examples in the following directory

    C:\Xilinx\Vitis\2021.1\data\embeddedsw\XilinxProcessorIPLib\drivers