Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Writing a custom Ethernet packet transmitter on PL side
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 494 views
  • Users 0 members are here
Related

Writing a custom Ethernet packet transmitter on PL side

e14 Contributor
e14 Contributor over 10 years ago

I started experimenting on the Zedboard recently. I want to implement a small design (as in, write VHDL code) which transmits a (hard coded for now) packet through the PHY layer (without using the PS). I don't need the receive part currently.

1)Is it possible to implement just the transmitter?

2)Also is it possible to do this purely from the PL layer (with VHDL code and constraint file), or is using the PS necessary?

I managed to switch values on 4 output pins at both rising and falling edges. (Don't know if it will violate any timing conditions at higher clock speeds).
In the Zedboard hardware user guide it is said that the TX clock is given by the PHY, so I thought i could just map my clock pin (input) there (right?).
And according to RGMII datasheet, I just need to transmit 11 or 00 on the TX_CTRL pin, to show if i am done transmitting or not.

But I don't see any pins for MDIO in the H/W user guide.

3)How do I configure the PHY then?

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    You will still need to implement a MAC in the PL.  If you intend to write your own, then I do not think this forum is the right place for support.  There is MAC ip in Vivado that you can use with a block design.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

    I am experimenting with Ethernet on the Zedboard as well.
    Unfortunately, your are NOT able to connect the PHY to the PL!

    On the Zedboard, the Marvell PHY is connected to one of the PS MACs via RGMII.

    The MAC then drops the Ethernet frames via DMA to the RAM, from where it can be accessed by the ARM Cores.

    **Important Note**: If you configure the PSs I/O, you will find the option to route the Eth0 to the EMIO Bank, which would allow access from the PL side.
    If you do this, this option will cut off the connection between MAC and PHY, giving the PL access only to the MAC via GMII, without any physical connection to the Ethernet port! This makes only sense if you are connecting an external PHY via FMC to the PL and want to use the PS MAC instead of writing your own!

    It took me a while to get that..

    cheers!