Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interfacing an Ultrasonic Rangefinder
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 509 views
  • Users 0 members are here
Related

Interfacing an Ultrasonic Rangefinder

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I'm having trouble interfacing an ultrasonic rangefinder pmod to the Zedboard.
My approach was to connect the ultrasonic rangefinder to the pmod inteface 'JA' and write the following code in the constraint file:
set_property PACKAGE_PIN C5  [get_ports {pwm_in}]
set_property IOSTANDARD LVCMOS33 [get_ports{pwml_in}]

When I synthesize the design, I'm getting an error that no 'object' has been defined for set_property.

I'm using Xilinx Vivado and trying to get the pwm signal from the pmod.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    That would depend on how you want to interface to the signal on the JA PMOD interface. If you want to use a GPIO interface you can either add an AXI GPIO IP block or connect to one of the PS GPIO via EMIO interface.

     

    Based on your questions I would suggest that you spend some time learning more about how the Zynq device and the Vivado tools work. The Avnet Zynq SW and HW Speedway workshops are a good place to start:

     

    http://zedboard.org/support/trainings-and-videos

     

    Or you could take a look at Adam Taylor's MicroZed Chronicles:

     

    http://zedboard.org/content/microzed-chronicles

     

    If you are a student the Xilinx University program material is also a place to start:

     

    http://www.xilinx.com/support/university.html

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    That would depend on how you want to interface to the signal on the JA PMOD interface. If you want to use a GPIO interface you can either add an AXI GPIO IP block or connect to one of the PS GPIO via EMIO interface.

     

    Based on your questions I would suggest that you spend some time learning more about how the Zynq device and the Vivado tools work. The Avnet Zynq SW and HW Speedway workshops are a good place to start:

     

    http://zedboard.org/support/trainings-and-videos

     

    Or you could take a look at Adam Taylor's MicroZed Chronicles:

     

    http://zedboard.org/content/microzed-chronicles

     

    If you are a student the Xilinx University program material is also a place to start:

     

    http://www.xilinx.com/support/university.html

     

    -Gary