Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interfacing an Ultrasonic Rangefinder
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 508 views
  • Users 0 members are here
Related

Interfacing an Ultrasonic Rangefinder

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I'm having trouble interfacing an ultrasonic rangefinder pmod to the Zedboard.
My approach was to connect the ultrasonic rangefinder to the pmod inteface 'JA' and write the following code in the constraint file:
set_property PACKAGE_PIN C5  [get_ports {pwm_in}]
set_property IOSTANDARD LVCMOS33 [get_ports{pwml_in}]

When I synthesize the design, I'm getting an error that no 'object' has been defined for set_property.

I'm using Xilinx Vivado and trying to get the pwm signal from the pmod.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    I see at least two issues.

     

    First, the signal names for your two 'set_property' statements do not match. I suspect that one of the signal names does not exist in your design, which would cause the error.

     

    Second, package pin C5 is on the JE PMOD interface, which is a 'PS' or MIO interface that is already assigned with a fixed 3.3V IO and would not need the declarations in the constraints file. I suspect you really want package pin AA9 on the JA PMOD interface.

     

    You might want to use the ZedBoard master constraints file as a starting point. Just delete or comment out any signals you are not using and rename the signals to match your design. You can download the master constraints file here:

     

    http://zedboard.org/support/documentation/1521

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you for the information about the master constraint file.

    In the block diagram that I create, do I need an AXI-GPIO IP block if I use the JA pmod interface?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    That would depend on how you want to interface to the signal on the JA PMOD interface. If you want to use a GPIO interface you can either add an AXI GPIO IP block or connect to one of the PS GPIO via EMIO interface.

     

    Based on your questions I would suggest that you spend some time learning more about how the Zynq device and the Vivado tools work. The Avnet Zynq SW and HW Speedway workshops are a good place to start:

     

    http://zedboard.org/support/trainings-and-videos

     

    Or you could take a look at Adam Taylor's MicroZed Chronicles:

     

    http://zedboard.org/content/microzed-chronicles

     

    If you are a student the Xilinx University program material is also a place to start:

     

    http://www.xilinx.com/support/university.html

     

    -Gary