Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ADAU1761 ALSAMIXER Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 508 views
  • Users 0 members are here
Related

ADAU1761 ALSAMIXER Xillinux

metinburak_
metinburak_ over 12 years ago

Hi,

Can we use aplay and arecord of Alsamixer with the Adau1761 chip? I built the Xillinux system but the alsamixer doesn't see any soundcard when i make aplay -l.

Only on graphical desktop i can play music by the help of pulseaudio. But i ll make use of a library which uses alsamixer and so the soundcard isn't working.

Anybody used the chip with alsamixer?

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • metinburak_
    0 metinburak_ over 12 years ago

    So should i use it as an AXI IIC module to use it with ALSA?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to metinburak_

    If you want to use the ALSA driver in the kernel, that requires reorganizing the PL part according to the schema offered by Analog Devices (in XPS + some HDL editing), and also set up the Device Tree to reflect the updated processor environment. I haven't looked much into this direction, so I can't comment more on this.

       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to metinburak_

    If you want to use the ALSA driver in the kernel, that requires reorganizing the PL part according to the schema offered by Analog Devices (in XPS + some HDL editing), and also set up the Device Tree to reflect the updated processor environment. I haven't looked much into this direction, so I can't comment more on this.

       Eli