Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ADAU1761 ALSAMIXER Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 499 views
  • Users 0 members are here
Related

ADAU1761 ALSAMIXER Xillinux

metinburak_
metinburak_ over 12 years ago

Hi,

Can we use aplay and arecord of Alsamixer with the Adau1761 chip? I built the Xillinux system but the alsamixer doesn't see any soundcard when i make aplay -l.

Only on graphical desktop i can play music by the help of pulseaudio. But i ll make use of a library which uses alsamixer and so the soundcard isn't working.

Anybody used the chip with alsamixer?

Thanks in advance.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    The support for audio on the Zedboard was made using a Xillybus device file (/dev/xillybus_audio) to communicate sample data with the FPGA, which in turn handles the interface with the audio chip. This is why there's no classic kernel driver, but only access through Pulseaudio.

    If that's possible, you may use Pulseaudio's interface (e.g. /dev/snd/), which isn't limited to the graphical desktop. Alternatively, you may find the padsp program useful for faking a classic /dev/dsp interface, if that helps.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • metinburak_
    0 metinburak_ over 12 years ago

    So should i use it as an AXI IIC module to use it with ALSA?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to metinburak_

    If you want to use the ALSA driver in the kernel, that requires reorganizing the PL part according to the schema offered by Analog Devices (in XPS + some HDL editing), and also set up the Device Tree to reflect the updated processor environment. I haven't looked much into this direction, so I can't comment more on this.

       Eli