Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Understanding Address Map
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 2863 views
  • Users 0 members are here
Related

Understanding Address Map

jmales
jmales over 11 years ago

Please refer to page 113 of http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

I'm not understanding this table. From what I can tell, I have from 0010_0000 to 3FFF_FFF of DDR memory, which is 1 072 693 247 bytes and approximately 1 Gbyte of memory available to write into the DDR, correct? I thought the Zedboard had only 512 Mbytes of DDR memory...

Also, in that table, it says that I have approximately 2Gbytes (4000_0000 to BFFF_FFFF) of address available for PL. What does this space mean exactly? What can I save in here?

Thank you

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    4G is the maximum addressable area given that there are 32 address bits. The table referred to by jmales above maps how that 4G of address space is allocated for use in the Zynq device.

    512M is the actual amount of DDR memory that is physically installed on the ZedBoard. Other Zynq based boards may have more, or less, DDR memory.

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    4G is the maximum addressable area given that there are 32 address bits. The table referred to by jmales above maps how that 4G of address space is allocated for use in the Zynq device.

    512M is the actual amount of DDR memory that is physically installed on the ZedBoard. Other Zynq based boards may have more, or less, DDR memory.

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    thx for your reply. i think i have understood this question by you help.

    BTW, i want to enable the two ethernet function  on my customize board. i can use it independently, but can not work up when both are enable. Do you have any advise or any material about this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    You will need to provide more detail about what you are trying to accomplish.

    Is your custom board an add-on board (FMC) to the ZedBoard or a completely custom Zynq based board. If so what Zynq device?

    Are you attempting to use the two Ethernet controllers in the Zynq PS (Processor System), PL (Programmable Logic) based Ethernet MACs, or a combination of both?

    Do the PHYs for your two Ethernet controllers share a common MDIO control path or are they separate?

    Are you attempting to get the ethernet channels to work in a 'bare metal' mode or using Linux or some other OS?

    These links may also be helpful as working examples of multiple ethernet ports on a ZedBoard:

    http://www.fpgadeveloper.com/category/tutorials

    http://ethernetfmc.com/

    -Gary