Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Understanding Address Map
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 2859 views
  • Users 0 members are here
Related

Understanding Address Map

jmales
jmales over 11 years ago

Please refer to page 113 of http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

I'm not understanding this table. From what I can tell, I have from 0010_0000 to 3FFF_FFF of DDR memory, which is 1 072 693 247 bytes and approximately 1 Gbyte of memory available to write into the DDR, correct? I thought the Zedboard had only 512 Mbytes of DDR memory...

Also, in that table, it says that I have approximately 2Gbytes (4000_0000 to BFFF_FFFF) of address available for PL. What does this space mean exactly? What can I save in here?

Thank you

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The Zynq TRM address map tables on page 113 indicate the addressable ranges available to the ARM CPUs and other Bus Masters within the Zynq device. These are the maximum address ranges assigned. They do not imply that a specific hardware implementation, such as the ZedBoard, actually completely fill these ranges. So, as you have noted, the ZedBoard only has 512 MBytes of DDR memory implemented on the board.

     

    The PL address range can be used by AXI peripherals and IP implemented in the Programmable Logic of the Zynq device. You might want to take a look at the Avnet Zynq HW and SW Speedway workshop material for a description of the Zynq memory areas and how to implement designs in the Zynq device.

     

    Developing ZynqRegistered-7000 All Programmable SoC Software (Vivado 2013.3 and 2014.4.1)

    Developing ZynqRegistered-7000 All Programmable SoC Hardware (Vivado 2013.3 and 2014.4.1)

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    sorry, i still not understand this question completely. i am confused about the 512M DDR Memory and 4G Address Map, what is the relation ship about the two concept.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    sorry, i still not understand this question completely. i am confused about the 512M DDR Memory and 4G Address Map, what is the relation ship about the two concept.