Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Create UART0 to PMOD (Rx, Tx)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1353 views
  • Users 0 members are here
Related

Create UART0 to PMOD (Rx, Tx)

Former Member
Former Member over 11 years ago

Hi everyone,
My problem is that I want create a serial interface with the Zedboard (Rev C).
I tried to find a tutorial, which helps to contact.
I work with XPS and I clicked under "System Assembly View" to I/O Peripherals and selected UART0 and MIO 10,11 (Is this realy a Pin or only an address?). I saw in an other tutorial where someone add an enet0. There was the next step to switch to the tab "Ports" and select to "make Ports external" but I have there no options.

What do I wrong? What is the next step? Can I write in system.ucf easily which PMOD Pin I want? For example:

net uart0_rx_pin LOC = Y11 | IOSTANDARD = LVCMOS33; # JA1
net uart0_tx_pin LOC = AA11 | IOSTANDARD = LVCMOS33; # JA2
(Must I write something to activate VCC and GND? Probably not, isn't it?)
I think, the next step will be to generate the NetList and the Bitstream and to export the hardware design to sdk.

There I read something about by the #define of the pins. Where I find this adresses?

Thanks for help.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    There are Zedboard based tutorials for both the Vivado and ISE/PlanAhead tools available here: http://zedboard.org/support/design/1521/11

     

    There are more in depth Speedway workshops that target the ZedBoard here: http://zedboard.org/support/trainings-and-videos

     

    If you choose to work with the Vivado tool suite there are also good blog and tutorial links:

     

    http://www.fpgadeveloper.com/category/tutorials

    http://svenand.blogdrive.com/archive/160.html#.VRle9I54o8k

    http://zedboard.org/content/microzed-chronicles-free-e-book-released

     

    I would recommend using the Vivado tools if possible as the ISE/PlanAhead tools are dated and all new material will target the Vivado suite.

     

    To answer your question, the MIO 10,11 pins you have selected are fixed signals routed to the JE1 PS PMOD port and, if you used the Zynq Board definition when you started your project, do not need additional constraints. If you select 'EMIO' as an option then you would need to add ports and set the constraints to route the signals to the desired PL PMOD pins. You do not need to 'activate' VCC or GND.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    There are Zedboard based tutorials for both the Vivado and ISE/PlanAhead tools available here: http://zedboard.org/support/design/1521/11

     

    There are more in depth Speedway workshops that target the ZedBoard here: http://zedboard.org/support/trainings-and-videos

     

    If you choose to work with the Vivado tool suite there are also good blog and tutorial links:

     

    http://www.fpgadeveloper.com/category/tutorials

    http://svenand.blogdrive.com/archive/160.html#.VRle9I54o8k

    http://zedboard.org/content/microzed-chronicles-free-e-book-released

     

    I would recommend using the Vivado tools if possible as the ISE/PlanAhead tools are dated and all new material will target the Vivado suite.

     

    To answer your question, the MIO 10,11 pins you have selected are fixed signals routed to the JE1 PS PMOD port and, if you used the Zynq Board definition when you started your project, do not need additional constraints. If you select 'EMIO' as an option then you would need to add ports and set the constraints to route the signals to the desired PL PMOD pins. You do not need to 'activate' VCC or GND.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data