Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design connection between CPU and PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 359 subscribers
  • Views 1964 views
  • Users 0 members are here
Related

connection between CPU and PL

Former Member
Former Member over 12 years ago

hi all!

My question is how can i send and recieve data through the CPU that in the board to the FPGA,when i use the Tera Term (for example) and i write the data on my PC. because i can program only the FPGA by IMPACT but i can't send data to the FPGA.

I have enother question when i write C code and running it on the CPU that in the board how can i send data to the pmod? I mean is there eny comand that can do that?

thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago +1
    In general the Zynq system talk between CPU and FPGA through Axi-bus. If you read the Axi documentation there are three types: Axi, Axi-lite and Axi-stream; each have different data rate and complexity…
  • Former Member
    Former Member over 12 years ago +1
    For sending one bit of data to pmod, there are a couple way of doing it. One is enable PS's EMIO and use constraint to connect the pin to a PMOD port. Check out Zedboard CTT (for Vivado 2013.2) chapter…
Parents
  • Former Member
    0 Former Member over 12 years ago

    For sending one bit of data to pmod, there are a couple way of doing it.  One is enable PS's EMIO and use constraint to connect the pin to a PMOD port.  Check out Zedboard CTT (for Vivado 2013.2) chapter 3.  The example use EMIO to connect to a button for input; but you can change the IO pin to output and constrain it to a pmod pin instead.  To program the port, when you export to SDK the Xilinx tool will generate driver for EMIO, and you can take a look at that to see how to write data to the EMIO port.

    A second method is also shown in chapter 3, which is using a AXI-GPIO.  You can map the GPIO pin to any of the PMOD port, LED or button for input or output.  To write C program for it, similar to before Xilinx tool generate drivers and provide sample code.  AXI-GPIO is the method I have being using to send output pin signals.

    Anyway, take a look at CTT and let me know if you have question. Also, if you want to use I2C, SPI, or UART for sending/receiving data through pmod, it's actually pretty easy too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    For sending one bit of data to pmod, there are a couple way of doing it.  One is enable PS's EMIO and use constraint to connect the pin to a PMOD port.  Check out Zedboard CTT (for Vivado 2013.2) chapter 3.  The example use EMIO to connect to a button for input; but you can change the IO pin to output and constrain it to a pmod pin instead.  To program the port, when you export to SDK the Xilinx tool will generate driver for EMIO, and you can take a look at that to see how to write data to the EMIO port.

    A second method is also shown in chapter 3, which is using a AXI-GPIO.  You can map the GPIO pin to any of the PMOD port, LED or button for input or output.  To write C program for it, similar to before Xilinx tool generate drivers and provide sample code.  AXI-GPIO is the method I have being using to send output pin signals.

    Anyway, take a look at CTT and let me know if you have question. Also, if you want to use I2C, SPI, or UART for sending/receiving data through pmod, it's actually pretty easy too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    How can i use that from UART. I mean how can i send data through pmod by using UART.

    About the first quastion could you tell me after i do the ip design how i send data, i mean in what way through the terminal or what?
    i'd appreciate if you could tell me the steps about making my custom peripheral from the begining until the connection to my PC by terminal in general.

    thanks    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer