Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 2nd Ethernet int to connect PS and PL vai GMII
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 2110 views
  • Users 0 members are here
Related

2nd Ethernet int to connect PS and PL vai GMII

e14 Contributor
e14 Contributor over 12 years ago

I redirected Ethernet 1 to PL according to this article http://zedboard.org/content/redirecting-peripherals-mio-emio

But I suppose it is not enough. It's necessary to modify Linux device tree and
1. add definition of the Ethernet 1 (it's simple)
2. tell Ethernet controller to get Rx/Tx clocks from EMIO - I do not have any idea how to do it.

Can you help with it?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The signals you redirected from Ethernet 1 to the PL are the interface from the MAC inside the Zynq Processor Section (PS) to a PHY that you will need to supply. Figure 16-8 in the Zynq-7000 AP SoC Technical Reference Manual (UG585) is a good illustraion.

     

    Just as the Ethernet 0 MAC on the ZedBoard is connected via the MIO pins to a Marvell PHY with an RGMII interface you will need to connect Ethernet 0 via the EMIO/Programmable Logic section via MII/GMII interface to an external PHY that you provide. On a ZedBoard that probably means adding an FMC daughter card with a PHY. Typically the board with the PHY will have an oscillator to generate clocks for the PHY which will in turn supply the required clocks to clock capable input pins on the Zynq programmable logic section. These are the signals you will connect to the Ethernet 1 MAC via EMIO.

     

    Here is an example of a ZedBoard compatible FMC PHY card: http://www.em.avnet.com/en-us/design/drc/Pages/ISM-Networking-FMC-Module.aspx

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The signals you redirected from Ethernet 1 to the PL are the interface from the MAC inside the Zynq Processor Section (PS) to a PHY that you will need to supply. Figure 16-8 in the Zynq-7000 AP SoC Technical Reference Manual (UG585) is a good illustraion.

     

    Just as the Ethernet 0 MAC on the ZedBoard is connected via the MIO pins to a Marvell PHY with an RGMII interface you will need to connect Ethernet 0 via the EMIO/Programmable Logic section via MII/GMII interface to an external PHY that you provide. On a ZedBoard that probably means adding an FMC daughter card with a PHY. Typically the board with the PHY will have an oscillator to generate clocks for the PHY which will in turn supply the required clocks to clock capable input pins on the Zynq programmable logic section. These are the signals you will connect to the Ethernet 1 MAC via EMIO.

     

    Here is an example of a ZedBoard compatible FMC PHY card: http://www.em.avnet.com/en-us/design/drc/Pages/ISM-Networking-FMC-Module.aspx

     

    -Gary