Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zynq XC7Z020-CLG484-1 PLL clock synthesis
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 357 views
  • Users 0 members are here
Related

Zynq XC7Z020-CLG484-1 PLL clock synthesis

metinburak_
metinburak_ over 10 years ago

Hi,

My application is about using the LVDS_25 feature for high speed communication (probably a SERDES or something else).
I use the PLLE2 primitive to synthesize a high frequency clock from the FCLK0 as an input clock.(or the clock conencted to Y9 which is 100Mhz). I saw that the capability of LVDS_25 pairs is about 950Mbps, but when i use PLLE2 to get an output differential clock of 400 Mhz, i see the amplitude is about 300mV for one end, and the receiver can not receive the data correctly. I know there is too much to talk about a perfect design to accomplish the LVDS_25 capabilities but, i want to learn the IC's capability in terms of its speed grade, to synthesize and transmit/receive these frequencies. I looked at nearly all the documentations but there is no statement like 'Zynq 7020 -1 speed grade PL side can transmit X Mhz'. I need this because i am designing a system which requires a high bandwidth and want to use the LVDS_25 pairs most efficiently (max frequency for each lane).

I accomplished to communicate in 350 Mhz, but higher than this, there exists corruption. (using 2 zedboards connected via cables - not FMC connectors together)

This is i think the most important feature of the PL side, and i will be pleased if someone has already has accomplished a data transfer in high speed and will publish some technical insight.

Regards,

Burak Metin

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    It seems that you are using a Zedboard.  What connectors are you using to wire between the two Zedboards?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    It seems that you are using a Zedboard.  What connectors are you using to wire between the two Zedboards?

    --Dan