Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Modifying a peripheral and adding new design files
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 1147 views
  • Users 0 members are here
Related

Modifying a peripheral and adding new design files

chipslinger
chipslinger over 13 years ago

I've gotten through a few of the tutorials. This has been challenging as there always seems to be some little thing that doesn't go correctly and I spend a bunch of time figuring out some obscure part of the toolset. It's very humbling. I'm not exactly proud of the time I've spent, but at least I've gotten somewhere. I haven't used the Xilinx toolset in a few years, which doesn't help.

I have a 32-address register bank defined and can access it via the SDK! Alright! I've edited the peripheral vhdl file (I call it bus_interface.vhd) and user_logic.vhd file and have created a third vhdl file with part of my logic. There are a bunch of other files that I need to add in later on after I've finished simulation. I'm using the peripheral file (bus_interface.vhd) as the top level file in my peripheral and have connected the sub-modules from within this file.

Now I'm stuck. I'm having difficulty figuring out:
1. How can I add in the new files (and in what tool)?
2. Are the files added into the library part or into the project?
3. How do I refresh the design so that the new files are actually integrated into the design?
4. How do I connect the device pins to the peripheral? (I think I just found a note that talks about this, but I thought I'd ask so that the response covers the full topic).

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • chipslinger
    0 chipslinger over 13 years ago

    Yes, I have looked at the tutorial. Very nicely done. I went through it carefully and it was very helpful. I don't think I could have gotten as far without having this as my guide.

    I probably did not explain what I'm doing very well.

    The tutorial shows how to create a simple register.

    What I did was take the generated register set, add in new i/o signals, new logic, and new components that are in separate files. So, what was once a register set, is now a series of peripherals, like SPI controllers, debounced i/o ports, etc... I guess I could incorporate all these into a single top level file, but it would be a mess. So, the peripheral, which was once two files, is now three files, and will eventually be maybe 10 files.

    Where and how do I add these files into the project?
    I'm also not clear on what steps actually "refresh" the project files. I'm presuming that the tools do some magic to refresh subdirectories, etc.... and if I just change the files, they won't necessarily be incorporated into a rebuild. I'd feel better if I understood a bit more about what's going on "under the hood." So, once they're added into the project, what do I need so that the systems is refreshed?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chipslinger
    0 chipslinger over 13 years ago

    Yes, I have looked at the tutorial. Very nicely done. I went through it carefully and it was very helpful. I don't think I could have gotten as far without having this as my guide.

    I probably did not explain what I'm doing very well.

    The tutorial shows how to create a simple register.

    What I did was take the generated register set, add in new i/o signals, new logic, and new components that are in separate files. So, what was once a register set, is now a series of peripherals, like SPI controllers, debounced i/o ports, etc... I guess I could incorporate all these into a single top level file, but it would be a mess. So, the peripheral, which was once two files, is now three files, and will eventually be maybe 10 files.

    Where and how do I add these files into the project?
    I'm also not clear on what steps actually "refresh" the project files. I'm presuming that the tools do some magic to refresh subdirectories, etc.... and if I just change the files, they won't necessarily be incorporated into a rebuild. I'd feel better if I understood a bit more about what's going on "under the hood." So, once they're added into the project, what do I need so that the systems is refreshed?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 13 years ago in reply to chipslinger

    I think I am on the same path as chipslinger. I modified the user_logic and the simple_register files to try and get a 32 bit port out for reading. I was not sure where the port would come out but was hoping that by creating a new top level in planahead, new ports would appear in the system_stub.vhd, but nothing appeared to change.

    My goal is to use the simple register design as a starting point to interface my vhdl code with the processor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to chipslinger

    In "Peripheral Implementation Support" tag, click the second item "Generate ISE and XST project file .....", and XPS will create a complete project which can be modified by ISE.
    Once u go back to ISE, I am sure u can do any complicated logic design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer