Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design SPI signals simulation
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 704 views
  • Users 0 members are here
Related

SPI signals simulation

e14 Contributor
e14 Contributor over 10 years ago

Hello Everybody,

I am configuring actually the SPI in order to get data from my image sensor, But I want to know before i send it to my image sensor if there is an option to simulate the signals( SCLK,SI,CS_N), I want be sure that i m sending the good command and data.

Also i have a constraint between (CS_N ,SCLK) for example i have to wait 10 cycle of SCLK after CS_N is asserted and and 10 cycles of SCLK before Cs_N is deasserted, i had to respect a delay between adresse and data i have to wait 3 system of clock.
So my second question is how can I ensure those constraints.

this is my code for 4 registres i am using an axi spi:
#include "xspi.h"
#include "xparameters.h"
#include "xil_printf.h"
#include <stdio.h>
#include "sleep.h"



//XSpiPs spi; // instance of spi

static XSpi_Config *config;
static XSpi instance;


u8 spi_initialisation(u32 spi_device_ID, u32 slavemask)
{
tXSpi_Initialize(&instance,XPAR_PS7_SPI_0_DEVICE_ID);
tXSpi_SetOptions(&instance, 1);
tXSpi_SetSlaveSelectReg(&instance, 1);
tXSpi_Start(&instance);
tXSpi_IntrGlobalDisable(&instance);
treturn(XST_SUCCESS);
}



void spi_singlwrite(u8 adresse_0,u8 adresse_1,u8 data_0,u8 data_1)
{
tint status;
tusleep(10);
t            XSpi_Reset(&instance);
t            spi_initialisation(XPAR_PS7_SPI_0_DEVICE_ID,1);
ttttu8 byte_0 = adresse_0;
ttttu8 byte_1 = adresse_1;
ttttu8 byte_2 = data_0;
ttttu8 byte_3 = data_1;
ttttu8 writebuffer[4] = {byte_0,byte_1,byte_2,byte_3};
ttttXSpi_SetSlaveSelectReg(&instance, 1);
tt        status = XSpi_Transfer(&instance, writebuffer, NULL ,sizeof(writebuffer));
tt        XSpi_SetSlaveSelectReg(&instance, 0);


tt           if (status == XST_DEVICE_IS_STOPPED)
tt               txil_printf("XST_DEVICE_IS_STOPPED.r
");
tt           if (status == XST_DEVICE_BUSY)
tt                   txil_printf("XST_DEVICE_BUSY.r
");
tt           if (status == XST_SPI_NO_SLAVE)
tt                   txil_printf("XST_SPI_NO_SLAVE.r
");

}

int main(void)
{

  xil_printf("config spi start r
");
  spi_initialisation(XPAR_PS7_SPI_0_DEVICE_ID,0);

  spi_singlwrite(0x80,0x00,0x00,0x02);
  usleep(10);
  spi_singlwrite(0x80,0x01,0x00,0x90);
  usleep(10);
  spi_singlwrite(0x81,0x00,0x00,0x02);
  usleep(10);
  spi_singlwrite(0x81,0x01,0x00,0x90);
  xil_printf("config spi fin r
");
  return(0);
}
Thank you for your help.
Best regards,
Anisse BELMAJY

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Gary,

    Thank you for your reply. I am trying to monitor my signals on ILA to get ensure that I am sending the right data.

    I hope that the provider has already implemented thoses timing restrictions. Because i am working with a camera HD and i m used to configure more than 200 registers.

    In HDL it will be quite hard to implement my own SPI for 235 registers.

    -Anisse

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Gary,

    Thank you for your reply. I am trying to monitor my signals on ILA to get ensure that I am sending the right data.

    I hope that the provider has already implemented thoses timing restrictions. Because i am working with a camera HD and i m used to configure more than 200 registers.

    In HDL it will be quite hard to implement my own SPI for 235 registers.

    -Anisse