Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Use an external clock signal on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 2535 views
  • Users 0 members are here
Related

Use an external clock signal on the zedboard

e14 Contributor
e14 Contributor over 12 years ago

Hi people, I have a big question. Is it possible to use an external clock signal in the ZedBoard PL part? Thanks for your help!!!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    From the ZedBoard Hardware Users Guide:

     

    2.5 Clock sources

    The Zynq-7000 AP SoC’s PS subsystem uses a dedicated 33.3333 MHz clock source, IC18, Fox 767-33.333333-12, with series termination. The PS infrastructure can generate up to four PLL-based clocks for the PL system. An on-board 100 MHz oscillator, IC17, Fox 767-100-136, supplies the PL subsystem clock input on bank 13, pin Y9.

     

    There are also two pairs of inputs from the FMC connector that are connected to clock capable inputs on the Zynq device:

    FMC_CLK0_P / FMC-CLK0_N and FMC_CLK1_P / FMC-CLK1_N ( use the 'P' input for a single ended clock source)

     

    And the JA PMOD connector has a pair of pins (JA4 and JA10) that are connected to clock capable inputs.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    From the ZedBoard Hardware Users Guide:

     

    2.5 Clock sources

    The Zynq-7000 AP SoC’s PS subsystem uses a dedicated 33.3333 MHz clock source, IC18, Fox 767-33.333333-12, with series termination. The PS infrastructure can generate up to four PLL-based clocks for the PL system. An on-board 100 MHz oscillator, IC17, Fox 767-100-136, supplies the PL subsystem clock input on bank 13, pin Y9.

     

    There are also two pairs of inputs from the FMC connector that are connected to clock capable inputs on the Zynq device:

    FMC_CLK0_P / FMC-CLK0_N and FMC_CLK1_P / FMC-CLK1_N ( use the 'P' input for a single ended clock source)

     

    And the JA PMOD connector has a pair of pins (JA4 and JA10) that are connected to clock capable inputs.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    great! thank you very much for your help!