Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Use an external clock signal on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 2526 views
  • Users 0 members are here
Related

Use an external clock signal on the zedboard

e14 Contributor
e14 Contributor over 12 years ago

Hi people, I have a big question. Is it possible to use an external clock signal in the ZedBoard PL part? Thanks for your help!!!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    From the ZedBoard Hardware Users Guide:

     

    2.5 Clock sources

    The Zynq-7000 AP SoC’s PS subsystem uses a dedicated 33.3333 MHz clock source, IC18, Fox 767-33.333333-12, with series termination. The PS infrastructure can generate up to four PLL-based clocks for the PL system. An on-board 100 MHz oscillator, IC17, Fox 767-100-136, supplies the PL subsystem clock input on bank 13, pin Y9.

     

    There are also two pairs of inputs from the FMC connector that are connected to clock capable inputs on the Zynq device:

    FMC_CLK0_P / FMC-CLK0_N and FMC_CLK1_P / FMC-CLK1_N ( use the 'P' input for a single ended clock source)

     

    And the JA PMOD connector has a pair of pins (JA4 and JA10) that are connected to clock capable inputs.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    great! thank you very much for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ashahsana
    0 ashahsana over 12 years ago

    Hello everyone
    I want to receive clock from FMC_CLK0_P / FMC-CLK0_N and FMC_CLK1_P / FMC-CLK1_N of 7z020 for my mezzanine card.
    Can anyone explain how is it possible.
    thanks in advance
    Sana

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to ashahsana

    As discussed in your other post, you will need to look at the documentation for the ZC702 board to determine the pin assignments and constraints needed to match the Xilinx ZC702 board.

     

     
      
       

     The Xilinx ZC702 board is supported on the Xilinx community forums: http://forums.xilinx.com/ but here are a couple of places to start:
         http://www.xilinx.com/support/documentation/boards_and_kits/zc702_zvik/ug850-zc702-eval-bd.pdf
          
         http://www.xilinx.com/support/index.html/content/xilinx/en/supportNav/boards_and_kits/zynq-7000_soc_boards_and_kits/zynq-7000_soc_zc702_evaluation_kit.html
          
         -Gary