Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Using the XADC with PMOD headers
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 1008 views
  • Users 0 members are here
Related

Using the XADC with PMOD headers

fknudsen
fknudsen over 8 years ago

Hello,

 

I am working on a project in which i need to measure an analog signal on the Zedboard, preferably on the PMOD header(s). Looking around the forums I have seen example guides for using the XADC interface to measure internal voltages/temperatures on the Zynq7 devices. However, things seem to get complicated/fuzzy when I try to find resources on measuring external voltages. I found this (https://cdn.instructables.com/ORIG/FRT/SYN1/IWMMH04D/FRTSYN1IWMMH04D.pdf) guide for using the Zybo XADC since it appears that the Zybo board has a direct connection between the PMOD and internal ADC, however I could not find whether this was also true for the Zedboard.

 

An additional issue I have is that i would like to get a 12-bit digital output from the XADC IP which I can use as input to other IPs.

 

So my question is essentially: Is it possible to measure voltage on the PMOD headers and is it possible to output that measurement on a 12-bit bus to the PL? 

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello fknudsen,

    Please ask any further questions over at the Digilent support forum as they are the point of contact for educational support.

    Zedboard does not have any XADC pins on any of the Pmods, however it does have its own XADC header populated.

    Please refer to pg 25 of the Zedboard HW User Guide http://zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v2_2.pdf

    Thank you,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello fknudsen,

    Please ask any further questions over at the Digilent support forum as they are the point of contact for educational support.

    Zedboard does not have any XADC pins on any of the Pmods, however it does have its own XADC header populated.

    Please refer to pg 25 of the Zedboard HW User Guide http://zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v2_2.pdf

    Thank you,

    Josh