Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zed Board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 360 subscribers
  • Views 4673 views
  • Users 0 members are here
Related

Zed Board

100aditya
100aditya over 9 years ago

Dear Sir/Madam,

                             In mine project i want to send data from ubuntu PC to ZedBoard using Wifi. I got one link http://zedboard.org/product/wilink-8-adaptor which talks about some kind of Wifi adpater for Micro-zed.

         Will this link and its given documents be seamlessly used with ZedBoard.

Regards

Aditya

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    I can't seem to be able to find the snap shots you are refering too. As a starter, which Vivado version are you using? Also which Tutorial version are you using, the 2014.4.1 or 2013.3 version?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Hi Josh,

                  I have downloaded two thing from the link:-- http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441?sid=91896 

    1-  Download the labs (Vivado 2013.3)

     2- Download the labs (Vivado 2014.4.1)

    Actually i have left mine lab right now. So details i will be giving you tomorrow. As i have mentioned that right now i am going through the speedway s/w tutorial. So i have downloaded one prebuit h/w from that link mentioned above and started following the instruction given in LAB 2 tutorial. If you can open the link then you can also find the Lab2 tutorial. The problem i told you already....In SDK, in project explorer winow   system.xml file is not getting opened and some error is coming and also z_system_wrapper.bit is not getting loaded.

      On mine Desktop ISE 14.2 is installed so i am using the SDK that has been installed with ISE 14.2...............If it is the version issue then should i install Vivado?? But why this should be issue as SDK is just eclipse driven s/w development environment???

    Regards

    Aditya    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Hi Josh,

                  I have downloaded two thing from the link:-- http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441?sid=91896 

    1-  Download the labs (Vivado 2013.3)

     2- Download the labs (Vivado 2014.4.1)

    Actually i have left mine lab right now. So details i will be giving you tomorrow. As i have mentioned that right now i am going through the speedway s/w tutorial. So i have downloaded one prebuit h/w from that link mentioned above and started following the instruction given in LAB 2 tutorial. If you can open the link then you can also find the Lab2 tutorial. The problem i told you already....In SDK, in project explorer winow   system.xml file is not getting opened and some error is coming and also z_system_wrapper.bit is not getting loaded.

      On mine Desktop ISE 14.2 is installed so i am using the SDK that has been installed with ISE 14.2...............If it is the version issue then should i install Vivado?? But why this should be issue as SDK is just eclipse driven s/w development environment???

    Regards

    Aditya