Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zed Board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 360 subscribers
  • Views 4663 views
  • Users 0 members are here
Related

Zed Board

100aditya
100aditya over 9 years ago

Dear Sir/Madam,

                             In mine project i want to send data from ubuntu PC to ZedBoard using Wifi. I got one link http://zedboard.org/product/wilink-8-adaptor which talks about some kind of Wifi adpater for Micro-zed.

         Will this link and its given documents be seamlessly used with ZedBoard.

Regards

Aditya

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    If you refer to the product brief you will see that it is Zedboard compatable. As far as the documentation goes, for the most part it targets the MicroZed. So you will not be able to "seamlessly" use those designs with the Zedboard, some modifications will have to be made.

    --Josh 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Hi Josh

                 Thaks for reply. You have mentioned that some modification will have to be done. Could you please suggest the kind of changes. The changes that need to be done,  is well obvious or subtle and if i start working on the basis of above link will i get success . Also i am new to Zync development environment ,, could younplease suggest me some links for kick start.....

     

    Regards

    Aditya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    For a good introduction into the Zynq development environment I would suggest you go through the ZynqHW and ZynqSW Speedways.

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-and-201441

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441

     

    As for using the Zedboard with WILINK8 I'd suggest using PMOD's JE and JD

    Here’s the pinout for the JE and JD connectors, here is the Pinout. 

    --Josh

     

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                               
                           

    *Predefined PS MIO peripheral function

      
       

    J3 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

    PS            MIO Pin

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    Zedboard Pmod-JE1           (PS Bank0)

      
       

    PMOD_D0

      
       

    1

      
       

    JE1

      
       

    MIO 13

      
       

    A6

      
       

    SDIO_D1

      
       

    PMOD_D1

      
       

    2

      
       

    JE2

      
       

    MIO 10

      
       

    G7

      
       

    SDIO_D0

      
       

    PMOD_D2

      
       

    3

      
       

    JE3

      
       

    MIO 11

      
       

    B4

      
       

    SDIO_CMD

      
       

    PMOD_D3

      
       

    4

      
       

    JE4

      
       

    MIO 12

      
       

    C5

      
       

    SDIO_CLK

      
       

    GND

      
       

    5

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JE7

      
       

    MIO 0

      
       

    G6

      
       

    WL_IRQ

      
       

    PMOD_D5

      
       

    8

      
       

    JE8

      
       

    MIO 9

      
       

    C4

      
       

    WLAN_EN_SOC

      
       

    PMOD_D6

      
       

    9

      
       

    JE9

      
       

    MIO 14

      
       

    B6

      
       

    SDIO_D2

      
       

    PMOD_D7

      
       

    10

      
       

    JE10

      
       

    MIO 15

      
       

    E6

      
       

    SDIO_D3

      
       

    GND

      
       

    11

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
                                       
       

    J1 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

     

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    ZedBoard    Pmod JD1                 (IO Bank13)

      
       

    PMOD_D0

      
       

    1

      
       

    JD1_P

      
       

     

      
       

    V7

      
       

    BT_HCI_CTS

      
       

    PMOD_D1

      
       

    2

      
       

    JD1_N

      
       

     

      
       

    W7

      
       

    BT_HCI_TX

      
       

    PMOD_D2

      
       

    3

      
       

    JD2_P

      
       

     

      
       

    V5

      
       

    BT_HCI_RX

      
       

    PMOD_D3

      
       

    4

      
       

    JD2_N

      
       

     

      
       

    V4

      
       

    BT_HCI_RTS

      
       

    GND

      
       

    5

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JD3_P

      
       

     

      
       

    W6

      
       

    BT_EN_SOC

      
       

    PMOD_D5

      
       

    8

      
       

    JD3_N

      
       

     

      
       

    W5

      
       

    BT_WAKE_HOST

      
       

    PMOD_D6

      
       

    9

      
       

    JD4_P

      
       

     

      
       

    U6

      
       

    WL_RS232_TX

      
       

    PMOD_D7

      
       

    10

      
       

    JD4_N

      
       

     

      
       

    U5

      
       

    WL_RS232_RX

      
       

    GND

      
       

    11

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Thanks Josh..........i will look into this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                  I am going through the tutorials that you suggested and it seems that it is really good and helpful. I am little relaxed now. But one thing that i am afraid and i want to ask here is that.......as i am very novice to Xilinx development environment....so after doing this tutorials for the above given two links, will i be able to start mine Zed Board Project or will i need some other exposure also apart from this tutorials that you have mentioned.???....Please comment on this.

     

    Thanks 

    Aditya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                      I was going through LAB 2 session of Softwrae flow link and i got some errors. Would you please help me out?? Here i am attached two snapshots which you can find out in the link :-http://zedboard.org/imce?app=ckeditor%7Csendto%40ckeditor_imceSendTo%7C&CKEditor=edit-comment-body-und-0-value&CKEditorFuncNum=2&langCode=en-gb.

    1. mine_project_snap_shot

    2.Tutorial_snap_shot

    So as per lab 2 once i imported the .xml file in SDK it show the window screen as per  "Tutorial_snap_shot" mentioned above. But I am not getting this.What i am getting is as per  mine_project_snap_shot. The two differences are :

    1- It is not able to open .xml file and showing the error that you can look into mine_project_snap_shot

    2. Z_system_wrapper.bit is not getting included in the Project window

    please tell me what is error behind this.

     

    Regards

    Aditya

     

     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    I can't seem to be able to find the snap shots you are refering too. As a starter, which Vivado version are you using? Also which Tutorial version are you using, the 2014.4.1 or 2013.3 version?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Hi Josh,

                  I have downloaded two thing from the link:-- http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441?sid=91896 

    1-  Download the labs (Vivado 2013.3)

     2- Download the labs (Vivado 2014.4.1)

    Actually i have left mine lab right now. So details i will be giving you tomorrow. As i have mentioned that right now i am going through the speedway s/w tutorial. So i have downloaded one prebuit h/w from that link mentioned above and started following the instruction given in LAB 2 tutorial. If you can open the link then you can also find the Lab2 tutorial. The problem i told you already....In SDK, in project explorer winow   system.xml file is not getting opened and some error is coming and also z_system_wrapper.bit is not getting loaded.

      On mine Desktop ISE 14.2 is installed so i am using the SDK that has been installed with ISE 14.2...............If it is the version issue then should i install Vivado?? But why this should be issue as SDK is just eclipse driven s/w development environment???

    Regards

    Aditya    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    Just for your clarification, the two labs you downloaded are the same labs just ran on different Vivado versions. I would suggest going through the 2014.4.1 version since it is utilizing a more updated version of the tool.

    For this lab you will need to update to the proper Vivado version that matches the lab you are doing. The reason why I stress the need to use the correct Vivado version for the lab is because the hardware export from Vivado to SDK has changed several times over the tool versions.

    You can find it at this link :  https://www.xilinx.com/support/download.html Please make sure during your Vivado installation you check the box that installs SDK as well. 

    As for any future projects, I would highly recommend utilizing Vivado design suite over Xilinx ISE design suite for any zynq based projects. You will find much more support doing so.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Hi Josh,

            Thanks Josh for mentoring me...i will look into this and let you know the results.

     

    Regards

    Aditya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>