Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zed Board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 340 subscribers
  • Views 3669 views
  • Users 0 members are here
Related

Zed Board

100aditya
100aditya over 9 years ago

Dear Sir/Madam,

                             In mine project i want to send data from ubuntu PC to ZedBoard using Wifi. I got one link http://zedboard.org/product/wilink-8-adaptor which talks about some kind of Wifi adpater for Micro-zed.

         Will this link and its given documents be seamlessly used with ZedBoard.

Regards

Aditya

  • Sign in to reply
  • Cancel
Parents
  • 100aditya
    0 100aditya over 9 years ago

    Hi Josh,

                  Now mine problem got resolved.Actually i found mine cable was faulty because of which USB-UART port was not showing up in the device manager. Next thing that i do not understand is following... I am proceeding with Lab 5 s/w tutorial. In this we have to do the Memory test. Again i just followed the lab instruction but i am getting different results. Here is the screen shot of lab 5 tutorial result after running the Memory_test :-

     --------------------Starting Memory Test Application----------------------------

    NOTE: This application runs with D-Cache disabled.As a result, cacheline requests will not be generated

    Testing memory region: ps7_ddr_0
        Memory Controller: ps7_ddr
             Base Address: 0x00100000
                     Size: 0x1ff00000 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    Testing memory region: ps7_ram_1
        Memory Controller: ps7_ram
             Base Address: 0xffff0000
                     Size: 0x0000fe00 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    ---------------------Memory Test Application Complete----------------------
     
    But when i am running i am getting the following results on mine SDK console:-
     
      -------------------------------Starting Memory Test Application---------------------------------
      NOTE: This application runs with D-Cache disabled.As a result, cacheline requests will not be generated
      Testing memory region: ps7_ddr_0
          Memory Controller: ps7_ddr
               Base Address: 0x00100000
                       Size: 0x1ff00000 bytes 
                32-bit test: PASSED!
                16-bit test: PASSED!
                 8-bit test: PASSED!
      Testing memory region: ps7_ram_1
          Memory Controller: ps7_ram
               Base Address: 0xffff0000
                       Size: 0x0000fe00 bytes 
                32-bit test: PASSED!
                16-bit test: PASSED!
                 8-bit test: PASSED!
      Testing memory region: axi_bram_ctrl_0
          Memory Controller: axi_bram_ctrl
               Base Address: 0x40000000
                       Size: 0x00002000 bytes 
                32-bit test: FAILED!
                16-bit test: FAILED!
                 8-bit test: FAILED!
      -----------------------Memory Test Application Complete----------------------
     
    So as you can notice evrything is fine ,but in lab tutorial there is no result for 
    memory region: axi_bram_ctrl_0 but when i am running the Memory test applicartion in which memmory region :axi_bram_ctrl_0 is being tested and result is FAILED. I want to know the reason behind this????
     
    Regards
    Aditya
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100aditya
    0 100aditya over 9 years ago

    Hi Josh,

                  Now mine problem got resolved.Actually i found mine cable was faulty because of which USB-UART port was not showing up in the device manager. Next thing that i do not understand is following... I am proceeding with Lab 5 s/w tutorial. In this we have to do the Memory test. Again i just followed the lab instruction but i am getting different results. Here is the screen shot of lab 5 tutorial result after running the Memory_test :-

     --------------------Starting Memory Test Application----------------------------

    NOTE: This application runs with D-Cache disabled.As a result, cacheline requests will not be generated

    Testing memory region: ps7_ddr_0
        Memory Controller: ps7_ddr
             Base Address: 0x00100000
                     Size: 0x1ff00000 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    Testing memory region: ps7_ram_1
        Memory Controller: ps7_ram
             Base Address: 0xffff0000
                     Size: 0x0000fe00 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    ---------------------Memory Test Application Complete----------------------
     
    But when i am running i am getting the following results on mine SDK console:-
     
      -------------------------------Starting Memory Test Application---------------------------------
      NOTE: This application runs with D-Cache disabled.As a result, cacheline requests will not be generated
      Testing memory region: ps7_ddr_0
          Memory Controller: ps7_ddr
               Base Address: 0x00100000
                       Size: 0x1ff00000 bytes 
                32-bit test: PASSED!
                16-bit test: PASSED!
                 8-bit test: PASSED!
      Testing memory region: ps7_ram_1
          Memory Controller: ps7_ram
               Base Address: 0xffff0000
                       Size: 0x0000fe00 bytes 
                32-bit test: PASSED!
                16-bit test: PASSED!
                 8-bit test: PASSED!
      Testing memory region: axi_bram_ctrl_0
          Memory Controller: axi_bram_ctrl
               Base Address: 0x40000000
                       Size: 0x00002000 bytes 
                32-bit test: FAILED!
                16-bit test: FAILED!
                 8-bit test: FAILED!
      -----------------------Memory Test Application Complete----------------------
     
    So as you can notice evrything is fine ,but in lab tutorial there is no result for 
    memory region: axi_bram_ctrl_0 but when i am running the Memory test applicartion in which memmory region :axi_bram_ctrl_0 is being tested and result is FAILED. I want to know the reason behind this????
     
    Regards
    Aditya