Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zed Board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 340 subscribers
  • Views 3684 views
  • Users 0 members are here
Related

Zed Board

100aditya
100aditya over 9 years ago

Dear Sir/Madam,

                             In mine project i want to send data from ubuntu PC to ZedBoard using Wifi. I got one link http://zedboard.org/product/wilink-8-adaptor which talks about some kind of Wifi adpater for Micro-zed.

         Will this link and its given documents be seamlessly used with ZedBoard.

Regards

Aditya

  • Sign in to reply
  • Cancel
Parents
  • 100aditya
    0 100aditya over 9 years ago
    Hi Josh,
                    Actually i was going through the s/w tutorial--> Lab 9(Dual Processor) ,in which under experiment no 2 , our task was to  ""Creating Bare-Metal Application Project for CPU1",. But when i tried to follow the instruction and craeted the BSP for CPU1 ,i got the following error. 
     
     
    14:40:01 ERROR :  [Hsi 55-1545] Problem running tcl command ::sw_standalone_amp_v3_11_a::generate : invalid command name "xget_libgen_proc_handle"
        while executing
    "xget_libgen_proc_handle"
        (procedure "::sw_standalone_amp_v3_11_a::generate" line 8)
        invoked from within
    "::sw_standalone_amp_v3_11_a::generate standalone_amp"
     [Hsi 55-1442] Error(s) while running TCL procedure generate()
    14:40:01 ERROR : Failed to generate BSP.
    14:40:01 INFO : BSP Project P/app_cpu1_bsp has been successfully migrated.
    14:41:10 ERROR :  [Hsi 55-1545] Problem running tcl command ::sw_standalone_amp_v3_11_a::generate : invalid command name "xget_libgen_proc_handle"
        while executing
    "xget_libgen_proc_handle"
        (procedure "::sw_standalone_amp_v3_11_a::generate" line 8)
        invoked from within
    "::sw_standalone_amp_v3_11_a::generate standalone_amp"
     [Hsi 55-1442] Error(s) while running TCL procedure generate()
    14:41:10 ERROR : Error generating bsp sources: Failed to generate BSP.
    14:41:10 ERROR : Failed to generate sources for BSP project app_cpu1_bsp
    org.eclipse.core.runtime.CoreException: Internal error occurred while generating bsp sources. Please check the SDK Log view for further details.
    at com.xilinx.sdk.sw.ui.handlers.RegenBspSourcesHandler.internalGenerateBsp(RegenBspSourcesHandler.java:178)
    at com.xilinx.sdk.sw.ui.handlers.RegenBspSourcesHandler.access$2(RegenBspSourcesHandler.java:163)
    at com.xilinx.sdk.sw.ui.handlers.RegenBspSourcesHandler$1$1.run(RegenBspSourcesHandler.java:131)
    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2345)
    at com.xilinx.sdk.sw.ui.handlers.RegenBspSourcesHandler$1.run(RegenBspSourcesHandler.java:135)
    at org.eclipse.jface.operation.ModalContext$ModalContextThread.run(ModalContext.java:121)
     
     
    Could u please tell me why this error is coming and what is the remedy of this.
     
    Regards
    Aditya
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                     One more information regarding the error that i posted you just above is:-- In the problem window proveded in the SDK GUI is is showing that  make:***No Rule to make target 'all'": as an error while creating the the BSP for CPU1.  While giving your advice you can also take this as consideration.

     

    Regards

    Aditya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                     One more information regarding the error that i posted you just above is:-- In the problem window proveded in the SDK GUI is is showing that  make:***No Rule to make target 'all'": as an error while creating the the BSP for CPU1.  While giving your advice you can also take this as consideration.

     

    Regards

    Aditya