Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Problem about Axi4-Stream and VDMA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1265 views
  • Users 0 members are here
Related

Problem about Axi4-Stream and VDMA

Former Member
Former Member over 13 years ago

   I have a simple design in which i want to transfer the video data to DDR memory using VDMA IP.  Since the video source has a XSVI interface but VDMA need an AXI-Stream interface, so i use a Video In to AXI4-Stream IP(I call it vid_in_axi4s) to connect them.  But there is no data in memory.  So i use chipscope to debug it.    First, i add an Integrated Logic Analyzer between the video source and the vid_in_axi4s,  and i can see the data flow in chipscope analyzeru3002 Second,  i add a chipscope axi monitor IP between vid_in_axi4s and VDMA,  but there is no data showing in analyzeru3002So i can make a conclusion that the problem is between vid_in_axi4s and VDMAu3002

    To debug the problem, i modified my designu3002 I  remove the other IPs except the video source  and  vid_in_axi4su3002 I make the vid_in_axi4s::M_AXIS_VDIEO ports External  and  Loc the tdata pin  in  LED IOB,  tready pin in one Button in UCF fileu3002 Only  when  i  pressed  the Button(tready pin location),  i  can  see the LED onu3002 

     So,  i  think  my problem is caused by the  AXI4-Stream interface ( the tready signal) u3002 It seems that  i need  to trigger  the vid_in_axi4s::M_AXIS_VIDEO::tready signal u3002 I  really have done some basic configuration about  the VDMAu3002 How can i solve this problem?!   Is the job of triggering the vid_in_axi4s::M_AXIS_VIDEO::tready signal  done by VDMA?!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    Yes you need to drive the fsync-signal for at least a clock cycle.
    When VDMA receives fsync, then tready gets asserted.

    Note that Xilinx has a working xsvi2axi core:
    http://www.xilinx.com/support/documentation/application_notes/xapp521_XSVI_AXI4.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    Yes you need to drive the fsync-signal for at least a clock cycle.
    When VDMA receives fsync, then tready gets asserted.

    Note that Xilinx has a working xsvi2axi core:
    http://www.xilinx.com/support/documentation/application_notes/xapp521_XSVI_AXI4.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data