Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design can I write my own SPI interface controller in VHDL only
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 372 views
  • Users 0 members are here
Related

can I write my own SPI interface controller in VHDL only

sunsun1437
sunsun1437 over 8 years ago

Hello,

I have one of Zedboard, i need to interface a external board which will be connected to the SPI interface. There are only a few input/output pins, clk, enable, data_latch, din, dout pins. Can I write my own SPI controller and using PLL to generate the 50 MHz SPI clock?  

I have no experience using the embedded on board CPU and using the SDK tool. Can I make it to work using hardware only (verilog/VHDL only) ? Since this task need to be done in a short period of time, the learning curve using the SDK and software development tool may take too long..

 

Thanks!

Sun

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Sun,

    My suggestion to you would be to review the two simple barmetal SPI controllers that control a PMOD application.

    Please refer to Tutorial 06 and Tutorial 07 located here http://picozed.org/support/design/13076/106

    These tutorials demonstrate the use of either a PS or a PL SPI Controller.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Sun,

    My suggestion to you would be to review the two simple barmetal SPI controllers that control a PMOD application.

    Please refer to Tutorial 06 and Tutorial 07 located here http://picozed.org/support/design/13076/106

    These tutorials demonstrate the use of either a PS or a PL SPI Controller.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • sunsun1437
    0 sunsun1437 over 8 years ago in reply to jafoste4

    Thank you so much for the reply, i will take a look at the tutorial.

    -Sun