Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Issues with HDMI reference designs in Vivado 2014.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 886 views
  • Users 0 members are here
Related

Issues with HDMI reference designs in Vivado 2014.4

e14 Contributor
e14 Contributor over 11 years ago

I was playing with two reference designs "HDMI Display Controller Tutorial" and "Bare Metal HDMI for ZedBoard with ADI IP and ADV7511", they work fine ONLY when I  run the PRE-BUILT bitstreams/projects. And they fail if try to build a project in Vivado 2014.4.


Can anybody help with that? See details below...
-----------
Bare Metal HDMI for ZedBoard with ADI IP and ADV7511 - when trying to create a project by running build.tcl I get an error:

ERROR: [BD 5-216] VLNV <xilinx.com:ip:processing_system7:5.3> is not supported for this version of the tools.The latest version is:5.5
ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

    while executing
"create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7"
    invoked from within
"set sys_ps7  [create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7]"
    (file "../../../projects/common/zed/zed_system_bd.tcl" line 46)

    while executing
"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"
    (file "system_bd.tcl" line 2)

    while executing
"source system_bd.tcl"
    (procedure "adi_project_create" line 56)
    invoked from within
"adi_project_create adv7511_zed"
    (file "./system_project.tcl" line 7)

-----------
HDMI Display Controller Tutorial - when trying to create ZED HDMI display core running zed_dmi_display.tcl I get the following error:

WARNING: [IP_Flow 19-2162] IP 'design_1_gnd_0' is locked:
* IP definition 'Constant (1.0)' for IP 'design_1_gnd_0' has a newer minor version in the IP Catalog.
Please select 'Report IP Status' from the 'Tools/Report' menu or run Tcl command 'report_ip_status' for more information.
ERROR: [BD 41-541] Parameter cannot be set on a locked block. The block 'gnd' is locked, because : * IP definition 'Constant (1.0)' for IP 'design_1_gnd_0' has a newer minor version in the IP Catalog.
Please select 'Report IP Status' from the 'Tools/Report' menu or run Tcl command 'report_ip_status' for more information.
ERROR: [BD 41-245] set_property error - Parameter cannot be set on a locked block. The block 'gnd' is locked, because: * IP definition 'Constant (1.0)' for IP 'design_1_gnd_0' has a newer minor version in the IP Catalog.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    This error is probably caused by not having a license for the Xilinx IP. See this post for more information and a link to download an evaluation license: http://zedboard.org/content/tutorial-zedboard-hdmi-display-controller

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    This error is probably caused by not having a license for the Xilinx IP. See this post for more information and a link to download an evaluation license: http://zedboard.org/content/tutorial-zedboard-hdmi-display-controller

     

    -Gary