Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Vivado Help on Zed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 553 views
  • Users 0 members are here
Related

Vivado Help on Zed

e14 Contributor
e14 Contributor over 10 years ago

Greetings everyone,

I'm working on a project with a ZedBoard, and I'm having a little trouble.  I'm primarily an embedded ARM developer, and I'm pretty to new Xilinx tools - and completely new to Vivado.  This is my first time using Zynq.

I've created a Block design that includes two AXI_Uart16550 cores and a clock wizard (the final design will include more uarts, but I'd like to get it working with two).  I need a very strange baud rate, which is the reason for the clock wiz.  During synthesis and implementation, I'm seeing some clocking failures and although I can produce a bitstream, things aren't working as I would expect.

Can anyone have a look at my vivado project and see if I've done something incorrectly?  I think I might have the processor resets wrong, but I'm not at all sure.

Any help would be greatly appreciated!

Vivado 2015.4 Project
https://file.io/d6cweS

James

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello James,

     

    Your link is broken.

     

    I would suggest adding your Zynq PS block and then your AXI Uart blocks to your block design and then using the 'Connection Automation' to generate the correct interconnection and resets.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello James,

     

    Your link is broken.

     

    I would suggest adding your Zynq PS block and then your AXI Uart blocks to your block design and then using the 'Connection Automation' to generate the correct interconnection and resets.

     

    -Gary